WDOG_TypeDef Struct ReferenceDevices > WDOG
WDOG Register Declaration
Definition at line 49
of file efm32gg11b_wdog.h
.
#include <
efm32gg11b_wdog.h
>
Data Fields | |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
WDOG_PCH_TypeDef | PCH [2] |
uint32_t | RESERVED0 [2] |
__IM uint32_t | SYNCBUSY |
Field Documentation
__IOM uint32_t WDOG_TypeDef::CMD |
__IOM uint32_t WDOG_TypeDef::CTRL |
Control Register
Definition at line 50
of file efm32gg11b_wdog.h
.
Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), and WDOGn_Lock().
__IOM uint32_t WDOG_TypeDef::IEN |
Interrupt Enable Register
Definition at line 61
of file efm32gg11b_wdog.h
.
Referenced by WDOGn_IntDisable(), WDOGn_IntEnable(), and WDOGn_IntGetEnabled().
__IM uint32_t WDOG_TypeDef::IF |
Watchdog Interrupt Flags
Definition at line 58
of file efm32gg11b_wdog.h
.
Referenced by WDOGn_IntGet(), and WDOGn_IntGetEnabled().
__IOM uint32_t WDOG_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 60
of file efm32gg11b_wdog.h
.
Referenced by WDOGn_IntClear().
__IOM uint32_t WDOG_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 59
of file efm32gg11b_wdog.h
.
Referenced by WDOGn_IntSet().
WDOG_PCH_TypeDef WDOG_TypeDef::PCH[2] |
PCH
Definition at line 55
of file efm32gg11b_wdog.h
.
uint32_t WDOG_TypeDef::RESERVED0[2] |
Reserved for future use
Definition at line 57
of file efm32gg11b_wdog.h
.
__IM uint32_t WDOG_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 53
of file efm32gg11b_wdog.h
.
Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), and WDOGn_Lock().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/
efm32gg11b_wdog.h