CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU
HFXO initialization structure. Init values should be obtained from a configuration tool, app note or xtal datasheet
Definition at line 1395
of file em_cmu.h
.
#include <
em_cmu.h
>
Data Fields | |
uint16_t | ctuneStartup |
uint16_t | ctuneSteadyState |
CMU_OscMode_TypeDef | mode |
uint8_t | timeoutPeakDetect |
uint8_t | timeoutStartup |
uint8_t | timeoutSteady |
uint16_t | xoCoreBiasTrimStartup |
uint16_t | xoCoreBiasTrimSteadyState |
Field Documentation
uint16_t CMU_HFXOInit_TypeDef::ctuneStartup |
Startup phase CTUNE (load capacitance) value
Definition at line 1397
of file em_cmu.h
.
Referenced by BSP_initClocks(), and CMU_HFXOInit().
uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState |
Steady-state phase CTUNE (load capacitance) value
Definition at line 1398
of file em_cmu.h
.
Referenced by BSP_initClocks(), and CMU_HFXOInit().
CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode |
uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect |
uint8_t CMU_HFXOInit_TypeDef::timeoutStartup |
uint8_t CMU_HFXOInit_TypeDef::timeoutSteady |
uint16_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup |
Startup XO core bias current trim
Definition at line 1399
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
uint16_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState |
Steady-state XO core bias current trim
Definition at line 1400
of file em_cmu.h
.
Referenced by CMU_HFXOInit().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_cmu.h