CAN_MessageObject_TypeDef Struct ReferenceEMLIB > CAN
CAN Message Object TypeDef structure. LSBs is used
Definition at line
126
of file
em_can.h
.
#include <
em_can.h
>
Data Fields |
|
| uint8_t | data [8] |
| bool | directionMask |
| uint8_t | dlc |
| bool | extended |
| bool | extendedMask |
| uint32_t | id |
| uint32_t | mask |
| uint8_t | msgNum |
Field Documentation
| uint8_t CAN_MessageObject_TypeDef::data[8] |
Pointer to the data, [0 - 8] bytes
Definition at line
143
of file
em_can.h
.
Referenced by CAN_ReadMessage() , and CAN_WriteData() .
| bool CAN_MessageObject_TypeDef::directionMask |
Enable the use of 'direction' value for filtering
Definition at line
152
of file
em_can.h
.
Referenced by CAN_SetIdAndFilter() .
| uint8_t CAN_MessageObject_TypeDef::dlc |
Data Length Code [0 - 8]
Definition at line
140
of file
em_can.h
.
Referenced by CAN_ReadMessage() , CAN_SendMessage() , and CAN_WriteData() .
| bool CAN_MessageObject_TypeDef::extended |
Id extended if true, standard if false
Definition at line
131
of file
em_can.h
.
Referenced by CAN_SendMessage() , and CAN_SetIdAndFilter() .
| bool CAN_MessageObject_TypeDef::extendedMask |
Enable the use of 'extended' value for filtering
Definition at line
149
of file
em_can.h
.
Referenced by CAN_SetIdAndFilter() .
| uint32_t CAN_MessageObject_TypeDef::id |
Id of the message, with 11 bits (standard) or 28 bits (extended). LSBs are used for both of them
Definition at line
137
of file
em_can.h
.
Referenced by CAN_SendMessage() , and CAN_SetIdAndFilter() .
| uint32_t CAN_MessageObject_TypeDef::mask |
Mask for id filtering
Definition at line
146
of file
em_can.h
.
Referenced by CAN_SetIdAndFilter() .
| uint8_t CAN_MessageObject_TypeDef::msgNum |
Message number of this Message Object, [1 - 32]
Definition at line
128
of file
em_can.h
.
Referenced by CAN_ReadMessage() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_can.h