LDMA_CH_TypeDef Struct ReferenceDevicesDevices > | LDMA

LDMA_CH LDMA CH Register


      

.

Definition at line 47 of file efm32gg11b_ldma_ch.h .

#include < efm32gg11b_ldma_ch.h >

Data Fields

__IOM uint32_t CFG
__IOM uint32_t CTRL
__IOM uint32_t DST
__IOM uint32_t LINK
__IOM uint32_t LOOP
__IOM uint32_t REQSEL
uint32_t RESERVED0 [5]
__IOM uint32_t SRC

Field Documentation

__IOM uint32_t LDMA_CH_TypeDef::CFG

Channel Configuration Register

Definition at line 49 of file efm32gg11b_ldma_ch.h .

__IOM uint32_t LDMA_CH_TypeDef::CTRL

Channel Descriptor Control Word Register

Definition at line 51 of file efm32gg11b_ldma_ch.h .

__IOM uint32_t LDMA_CH_TypeDef::DST

Channel Descriptor Destination Data Address Register

Definition at line 53 of file efm32gg11b_ldma_ch.h .

__IOM uint32_t LDMA_CH_TypeDef::LINK

Channel Descriptor Link Structure Address Register

Definition at line 54 of file efm32gg11b_ldma_ch.h .

__IOM uint32_t LDMA_CH_TypeDef::LOOP

Channel Loop Counter Register

Definition at line 50 of file efm32gg11b_ldma_ch.h .

__IOM uint32_t LDMA_CH_TypeDef::REQSEL

Channel Peripheral Request Select Register

Definition at line 48 of file efm32gg11b_ldma_ch.h .

uint32_t LDMA_CH_TypeDef::RESERVED0[5]

Reserved future

Definition at line 55 of file efm32gg11b_ldma_ch.h .

__IOM uint32_t LDMA_CH_TypeDef::SRC

Channel Descriptor Source Data Address Register

Definition at line 52 of file efm32gg11b_ldma_ch.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/ efm32gg11b_ldma_ch.h