LEUART_TypeDef Struct ReferenceDevices > LEUART

LEUART Register Declaration

Definition at line 49 of file efm32gg11b_leuart.h .

#include < efm32gg11b_leuart.h >

Data Fields

__IOM uint32_t CLKDIV
__IOM uint32_t CMD
__IOM uint32_t CTRL
__IOM uint32_t FREEZE
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t INPUT
__IOM uint32_t PULSECTRL
uint32_t RESERVED0 [3]
uint32_t RESERVED1 [2]
__IOM uint32_t ROUTELOC0
__IOM uint32_t ROUTEPEN
__IM uint32_t RXDATA
__IM uint32_t RXDATAX
__IM uint32_t RXDATAXP
__IOM uint32_t SIGFRAME
__IOM uint32_t STARTFRAME
__IM uint32_t STATUS
__IM uint32_t SYNCBUSY
__IOM uint32_t TXDATA
__IOM uint32_t TXDATAX

Field Documentation

__IOM uint32_t LEUART_TypeDef::CLKDIV

Clock Control Register

Definition at line 53 of file efm32gg11b_leuart.h .

Referenced by LEUART_BaudrateGet() , LEUART_BaudrateSet() , and LEUART_Reset() .

__IOM uint32_t LEUART_TypeDef::CMD

Command Register

Definition at line 51 of file efm32gg11b_leuart.h .

Referenced by LEUART_Enable() , LEUART_Init() , LEUART_Reset() , LEUART_RxDmaInEM2Enable() , LEUART_TxDmaInEM2Enable() , and UARTDRV_InitLeuart() .

__IOM uint32_t LEUART_TypeDef::CTRL

Control Register

Definition at line 50 of file efm32gg11b_leuart.h .

Referenced by LEUART_Init() , LEUART_Reset() , LEUART_RxDmaInEM2Enable() , and LEUART_TxDmaInEM2Enable() .

__IOM uint32_t LEUART_TypeDef::FREEZE

Freeze Register

Definition at line 67 of file efm32gg11b_leuart.h .

Referenced by LEUART_FreezeEnable() .

__IOM uint32_t LEUART_TypeDef::IEN

Interrupt Enable Register

Definition at line 64 of file efm32gg11b_leuart.h .

Referenced by LEUART_IntDisable() , LEUART_IntEnable() , LEUART_IntGetEnabled() , and LEUART_Reset() .

__IM uint32_t LEUART_TypeDef::IF

Interrupt Flag Register

Definition at line 61 of file efm32gg11b_leuart.h .

Referenced by LEUART_IntGet() , and LEUART_IntGetEnabled() .

__IOM uint32_t LEUART_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 63 of file efm32gg11b_leuart.h .

Referenced by LEUART_IntClear() , and LEUART_Reset() .

__IOM uint32_t LEUART_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 62 of file efm32gg11b_leuart.h .

Referenced by LEUART_IntSet() .

__IOM uint32_t LEUART_TypeDef::INPUT

LEUART Input Register

Definition at line 74 of file efm32gg11b_leuart.h .

__IOM uint32_t LEUART_TypeDef::PULSECTRL

Pulse Control Register

Definition at line 65 of file efm32gg11b_leuart.h .

Referenced by LEUART_Reset() .

uint32_t LEUART_TypeDef::RESERVED0[3]

Reserved for future use

Definition at line 70 of file efm32gg11b_leuart.h .

uint32_t LEUART_TypeDef::RESERVED1[2]

Reserved for future use

Definition at line 73 of file efm32gg11b_leuart.h .

__IOM uint32_t LEUART_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 72 of file efm32gg11b_leuart.h .

Referenced by LEUART_Reset() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .

__IOM uint32_t LEUART_TypeDef::ROUTEPEN

I/O Routing Pin Enable Register

Definition at line 71 of file efm32gg11b_leuart.h .

Referenced by LEUART_Reset() , RETARGET_SerialInit() , and UARTDRV_InitLeuart() .

__IM uint32_t LEUART_TypeDef::RXDATA

Receive Buffer Data Register

Definition at line 57 of file efm32gg11b_leuart.h .

Referenced by LEUART_Rx() , and LEUART_RxDataGet() .

__IM uint32_t LEUART_TypeDef::RXDATAX

Receive Buffer Data Extended Register

Definition at line 56 of file efm32gg11b_leuart.h .

Referenced by LEUART_RxDataXGet() , and LEUART_RxExt() .

__IM uint32_t LEUART_TypeDef::RXDATAXP

Receive Buffer Data Extended Peek Register

Definition at line 58 of file efm32gg11b_leuart.h .

__IOM uint32_t LEUART_TypeDef::SIGFRAME

Signal Frame Register

Definition at line 55 of file efm32gg11b_leuart.h .

Referenced by LEUART_Reset() .

__IOM uint32_t LEUART_TypeDef::STARTFRAME

Start Frame Register

Definition at line 54 of file efm32gg11b_leuart.h .

Referenced by LEUART_Reset() .

__IM uint32_t LEUART_TypeDef::STATUS

Status Register

Definition at line 52 of file efm32gg11b_leuart.h .

Referenced by LEUART_Rx() , LEUART_RxDmaInEM2Enable() , LEUART_RxExt() , LEUART_StatusGet() , LEUART_Tx() , LEUART_TxDmaInEM2Enable() , and LEUART_TxExt() .

__IM uint32_t LEUART_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 68 of file efm32gg11b_leuart.h .

Referenced by LEUART_FreezeEnable() , and UARTDRV_InitLeuart() .

__IOM uint32_t LEUART_TypeDef::TXDATA

Transmit Buffer Data Register

Definition at line 60 of file efm32gg11b_leuart.h .

Referenced by LEUART_Tx() .

__IOM uint32_t LEUART_TypeDef::TXDATAX

Transmit Buffer Data Extended Register

Definition at line 59 of file efm32gg11b_leuart.h .

Referenced by LEUART_TxExt() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/ efm32gg11b_leuart.h