Cluster Commands: BACnet Protocol Tunnel
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_BACNET_PROTOCOL_TUNNEL_ZCL_BACNET_TRANSFER_NPDU_WHOIS |
zcl bacnet transfer-npdu whois | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_B_A_CNET_PROTOCOL_TUNNEL_RANDOM |
zcl bacnet transfer-npdu random [npdu:1] |
Detailed Description
This group describes the CLI commands for the BACnet Protocol Tunnel cluster. Listed below is a description of the cluster:
Commands and attributes required to tunnel the BACnet protocol.
Macro Definition Documentation
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_B_A_CNET_PROTOCOL_TUNNEL_RANDOM
#define EMBER_AF_DOXYGEN_CLI_COMMAND_B_A_CNET_PROTOCOL_TUNNEL_RANDOM |
zcl bacnet transfer-npdu random [npdu:1]
- This command is generated when a BACnet network layer wishes to transfer a BACnet NPDU across a ZigBee tunnel to another BACnet network layer.
- npdu - DATA8
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_BACNET_PROTOCOL_TUNNEL_ZCL_BACNET_TRANSFER_NPDU_WHOIS
#define EMBER_AF_DOXYGEN_CLI_COMMAND_BACNET_PROTOCOL_TUNNEL_ZCL_BACNET_TRANSFER_NPDU_WHOIS |
zcl bacnet transfer-npdu whois
- Send a sample whois command.