Functions

void halMicrophoneCodecMsadpcmDataReadyCallback (uint8_t *data, uint8_t length)
Called when new microphone data is ready.

Detailed Description

These callbacks are contributed by the Microphone Codec MSADPCM plugin.

Function Documentation

◆ halMicrophoneCodecMsadpcmDataReadyCallback()

void halMicrophoneCodecMsadpcmDataReadyCallback ( uint8_t * data,
uint8_t length
)

Called when new microphone data is ready.

This function is called by the plugin when new data has been processed and is ready to be processed by other parts of the system.

Parameters
data Pointer to the data that is ready.
length Length of the data.