A data structure used to describe the time in a human understandable format (as opposed to 32-bit UTC)
#include <af-types.h
>
A data structure used to describe the time in a human understandable format (as opposed to 32-bit UTC)
◆ day
uint8_t EmberAfTimeStruct::day |
◆ hours
uint8_t EmberAfTimeStruct::hours |
◆ minutes
uint8_t EmberAfTimeStruct::minutes |
◆ month
uint8_t EmberAfTimeStruct::month |
◆ seconds
uint8_t EmberAfTimeStruct::seconds |
◆ year
uint16_t EmberAfTimeStruct::year |
The documentation for this struct was generated from the following file: