#include < af-types.h >

Data Fields

EmberAfDeviceManagementTenancy tenancy
EmberAfDeviceManagementSupplier supplier
EmberAfDeviceManagementSupply supply
EmberAfDeviceManagementSiteId siteId
EmberAfDeviceManagementCIN cin
EmberAfDeviceManagementSupplyStatusFlags supplyStatusFlags
EmberAfDeviceManagementSupplyStatus supplyStatus
EmberAfDeviceManagementPassword servicePassword
EmberAfDeviceManagementPassword consumerPassword
EmberAfDeviceManagementUncontrolledFlowThreshold threshold
uint32_t providerId
uint32_t issuerEventId
uint8_t proposedLocalSupplyStatus
EmberAfTariffType tariffType
EmberAfDeviceManagementChangePendingFlags pendingUpdates

Field Documentation

cin

EmberAfDeviceManagementCIN EmberAfDeviceManagementInfo::cin

consumerPassword

EmberAfDeviceManagementPassword EmberAfDeviceManagementInfo::consumerPassword

issuerEventId

uint32_t EmberAfDeviceManagementInfo::issuerEventId

pendingUpdates

EmberAfDeviceManagementChangePendingFlags EmberAfDeviceManagementInfo::pendingUpdates

proposedLocalSupplyStatus

uint8_t EmberAfDeviceManagementInfo::proposedLocalSupplyStatus

providerId

uint32_t EmberAfDeviceManagementInfo::providerId

servicePassword

EmberAfDeviceManagementPassword EmberAfDeviceManagementInfo::servicePassword

siteId

EmberAfDeviceManagementSiteId EmberAfDeviceManagementInfo::siteId

supplier

EmberAfDeviceManagementSupplier EmberAfDeviceManagementInfo::supplier

supply

EmberAfDeviceManagementSupply EmberAfDeviceManagementInfo::supply

supplyStatus

EmberAfDeviceManagementSupplyStatus EmberAfDeviceManagementInfo::supplyStatus

supplyStatusFlags

EmberAfDeviceManagementSupplyStatusFlags EmberAfDeviceManagementInfo::supplyStatusFlags

tariffType

EmberAfTariffType EmberAfDeviceManagementInfo::tariffType

tenancy

EmberAfDeviceManagementTenancy EmberAfDeviceManagementInfo::tenancy

threshold

EmberAfDeviceManagementUncontrolledFlowThreshold EmberAfDeviceManagementInfo::threshold

The documentation for this struct was generated from the following file:
  • af-types.h