EmberAfDeviceManagementCIN Struct Reference
#include <
af-types.h
>
Data Fields |
|
uint8_t | cin [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH +1] |
uint32_t | implementationDateTime |
uint32_t | issuerEventId |
Field Documentation
◆ cin
uint8_t EmberAfDeviceManagementCIN::cin[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH +1] |
◆ implementationDateTime
uint32_t EmberAfDeviceManagementCIN::implementationDateTime |
◆ issuerEventId
uint32_t EmberAfDeviceManagementCIN::issuerEventId |
The documentation for this struct was generated from the following file:
-
af-types.h