Plugin Commands: APS Link Key Authorization
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ADD_CLUSTER_EXEMPTED |
plugin aps-link-key-auth add-cluster-exempted [cluster:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_CLEAR_EXEMPT_LIST |
plugin aps-link-key-auth clear-exempt-list | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ENABLE |
plugin aps-link-key-auth enable [enable:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ENABLE_WITH_EXEMPT_LIST |
plugin aps-link-key-auth enable-with-exempt-list [enable:1] [exemptClusterList:2] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_INFO |
plugin aps-link-key-auth info |
Detailed Description
This plugin provides a set of APIs and CLI commands for managing APS link key authorization
Macro Definition Documentation
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ADD_CLUSTER_EXEMPTED
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ADD_CLUSTER_EXEMPTED |
plugin aps-link-key-auth add-cluster-exempted [cluster:2]
- Adds an entry to the cluster exempt list.
- cluster - INT16U - Cluster to be added to the exempt list.
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_CLEAR_EXEMPT_LIST
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_CLEAR_EXEMPT_LIST |
plugin aps-link-key-auth clear-exempt-list
- Clears the exempt list.
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ENABLE
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ENABLE |
plugin aps-link-key-auth enable [enable:1]
- Enable or disable APS link key authorization for all clusters.
- enable - INT8U - Set the enable state of the APS link key security.
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ENABLE_WITH_EXEMPT_LIST
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_ENABLE_WITH_EXEMPT_LIST |
plugin aps-link-key-auth enable-with-exempt-list [enable:1] [exemptClusterList:2]
- Enables or disables APS link key authorization and setup the exempt list.
- enable - INT8U - Set the enable state of the APS link key security.
- exemptClusterList - INT16U - List of exempted clusters.
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_INFO
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_APS_LINK_KEY_AUTHORIZATION_PLUGIN_APS_LINK_KEY_AUTH_INFO |
plugin aps-link-key-auth info
- List information on the current state of APS link key authorization.