Plugin Commands: MPSI
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_RECEIVE_MESSAGE |
plugin mpsi receive-message [destinationAppId:1] [messageId:2] [payloadLength:1] [payload:-1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_SEND_MESSAGE |
plugin mpsi send-message [destinationAppId:1] [messageId:2] [payloadLength:1] [payload:-1] |
Detailed Description
This plugin provides a set of CLI commands to interact with the MPSI plugin.
Macro Definition Documentation
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_RECEIVE_MESSAGE
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_RECEIVE_MESSAGE |
plugin mpsi receive-message [destinationAppId:1] [messageId:2] [payloadLength:1] [payload:-1]
- Simulate receiving an MPSI message.
- destinationAppId - INT8U - The application ID of the message
- messageId - INT16U - The message ID of the message
- payloadLength - INT8U - The payload length of the message
- payload - OCTET_STRING - The payload of the message. This represents a serialized specific MPSI message.
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_SEND_MESSAGE
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MPSI_PLUGIN_MPSI_SEND_MESSAGE |
plugin mpsi send-message [destinationAppId:1] [messageId:2] [payloadLength:1] [payload:-1]
- Simulate sending an MPSI message.
- destinationAppId - INT8U - The application ID of the message
- messageId - INT16U - The message ID of the message
- payloadLength - INT8U - The payload length of the message
- payload - OCTET_STRING - The payload of the message. This represents a serialized specific MPSI message.