Functions

void emberAfPluginCoulombCounterEventCallback (uint32_t mask, uint32_t options)
Set the Radio states and energy modes.

Detailed Description

These callbacks are contributed by the Radio Coexistence Stub plugin.

Function Documentation

◆ emberAfPluginCoulombCounterEventCallback()

void emberAfPluginCoulombCounterEventCallback ( uint32_t mask,
uint32_t options
)

Set the Radio states and energy modes.

This function is called by the RAIL library to set the radio states for the purpose of coulomb counter, to indicate Idle/Rx/Tx. Also the Zigbee stack will call into this function to set the various energy modes.