Plugin Commands: Calendar Common

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_ADD_CAL_INFO
plugin calendar-common add-cal-info [providerId:4] [issuerEventId:4] [calId:4] [startTime:4] [calType:1] [calName:-1] [numberOfSeasons:1] [numberOfWeekProfiles:1] [numberOfDayProfiles:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_CLEAR
plugin calendar-common clear
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_ENHANCED_CALENDAR
plugin calendar-common load-enhanced-calendar [index:1] [providerId:4] [issuerEventId:4] [issuerCalendarId:4] [startTime:4] [type:1] [name:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_ENHANCED_SPECIAL_DAYS
plugin calendar-common load-enhanced-special-days [index:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_FLAT_CALENDAR
plugin calendar-common load-flat-calendar [index:1] [providerId:4] [issuerEventId:4] [issuerCalendarId:4] [startTime:4] [type:1] [name:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_SIMPLE_CALENDAR
plugin calendar-common load-simple-calendar [index:1] [providerId:4] [issuerEventId:4] [issuerCalendarId:4] [startTime:4] [type:1] [name:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_SIMPLE_SPECIAL_DAYS
plugin calendar-common load-simple-special-days [index:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_DAYS
plugin calendar-common print days
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SEASONS
plugin calendar-common print seasons
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SPECIAL_DAYS
plugin calendar-common print special-days
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SUMMARY
plugin calendar-common print summary
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_WEEKS
plugin calendar-common print weeks
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SELECT
plugin calendar-common select [index:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_CAL_INFO
plugin calendar-common set-cal-info [index:1] [providerId:4] [issuerEventId:4] [calId:4] [startTime:4] [calType:1] [calName:-1] [numberOfSeasons:1] [numberOfWeekProfiles:1] [numberOfDayProfiles:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_DAY_PROF_INFO
plugin calendar-common set-day-prof-info [index:1] [dayId:1] [entryId:1] [minutesFromMidnight:2] [data:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_SEASONS_INFO
plugin calendar-common set-seasons-info [index:1] [weekId:1] [startDate:4] [weekIdRef:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_WEEK_PROF_INFO
plugin calendar-common set-week-prof-info [index:1] [weekId:1] [dayIdRefMon:1] [dayIdRefTue:1] [dayIdRefWed:1] [dayIdRefThu:1] [dayIdRefFri:1] [dayIdRefSat:1] [dayIdRefSun:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_TEST_INIT
plugin calendar-common test-init

Detailed Description

The calendar common plugin commands provide commands to view and manipulate the local copy of the calendar.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_ADD_CAL_INFO

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_ADD_CAL_INFO

plugin calendar-common add-cal-info [providerId:4] [issuerEventId:4] [calId:4] [startTime:4] [calType:1] [calName:-1] [numberOfSeasons:1] [numberOfWeekProfiles:1] [numberOfDayProfiles:1]

  • Adding calendar information.
    • providerId - INT32U
    • issuerEventId - INT32U
    • calId - INT32U
    • startTime - INT32U
    • calType - INT8U
    • calName - OCTET_STRING
    • numberOfSeasons - INT8U
    • numberOfWeekProfiles - INT8U
    • numberOfDayProfiles - INT8U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_CLEAR

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_CLEAR

plugin calendar-common clear

  • Clear the calendars.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_ENHANCED_CALENDAR

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_ENHANCED_CALENDAR

plugin calendar-common load-enhanced-calendar [index:1] [providerId:4] [issuerEventId:4] [issuerCalendarId:4] [startTime:4] [type:1] [name:-1]

  • Loads the Enhanced Calendar defined in Appendix D.2 in the SE 1.2 Test specification.
    • index - INT8U - The index in the internal calendar table where this calendar is to be stored
    • providerId - INT32U - The provider ID
    • issuerEventId - INT32U - The issuer event ID
    • issuerCalendarId - INT32U - The issuer calendar ID
    • startTime - INT32U - The time when this calendar is to be considered active
    • type - INT8U - The type: Del=0x00, Rec=0x01, DelAndRec=0x02, Friendly=0x03, Aux=0x04
    • name - OCTET_STRING - The calendar name

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_ENHANCED_SPECIAL_DAYS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_ENHANCED_SPECIAL_DAYS

plugin calendar-common load-enhanced-special-days [index:1]

  • Loads the Simple Special Days defined in Appendix D.5 in the SE 1.2 Test specification.
    • index - INT8U - The index in the internal calendar table where the speical days are to be stored

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_FLAT_CALENDAR

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_FLAT_CALENDAR

plugin calendar-common load-flat-calendar [index:1] [providerId:4] [issuerEventId:4] [issuerCalendarId:4] [startTime:4] [type:1] [name:-1]

  • Loads the Flat Calendar defined in Appendix D.3 in the SE 1.2 Test specification.
    • index - INT8U - The index in the internal calendar table where this calendar is to be stored
    • providerId - INT32U - The provider ID
    • issuerEventId - INT32U - The issuer event ID
    • issuerCalendarId - INT32U - The issuer calendar ID
    • startTime - INT32U - The time when this calendar is to be considered active
    • type - INT8U - The type: Del=0x00, Rec=0x01, DelAndRec=0x02, Friendly=0x03, Aux=0x04
    • name - OCTET_STRING - The calendar name

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_SIMPLE_CALENDAR

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_SIMPLE_CALENDAR

plugin calendar-common load-simple-calendar [index:1] [providerId:4] [issuerEventId:4] [issuerCalendarId:4] [startTime:4] [type:1] [name:-1]

  • Loads the Simple Calendar defined in Appendix D.1 in the SE 1.2 Test specification.
    • index - INT8U - The index in the internal calendar table where this calendar is to be stored
    • providerId - INT32U - The provider ID
    • issuerEventId - INT32U - The issuer event ID
    • issuerCalendarId - INT32U - The issuer calendar ID
    • startTime - INT32U - The time when this calendar is to be considered active
    • type - INT8U - The type: Del=0x00, Rec=0x01, DelAndRec=0x02, Friendly=0x03, Aux=0x04
    • name - OCTET_STRING - The calendar name

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_SIMPLE_SPECIAL_DAYS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_LOAD_SIMPLE_SPECIAL_DAYS

plugin calendar-common load-simple-special-days [index:1]

  • Loads the Simple Special Days defined in Appendix D.4 in the SE 1.2 Test specification.
    • index - INT8U - The index in the internal calendar table where the speical days are to be stored

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_DAYS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_DAYS

plugin calendar-common print days

  • Prints the local calendar's days

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SEASONS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SEASONS

plugin calendar-common print seasons

  • Prints the local calendar's seasons.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SPECIAL_DAYS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SPECIAL_DAYS

plugin calendar-common print special-days

  • Prints the local calendar's special days.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SUMMARY

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_SUMMARY

plugin calendar-common print summary

  • Prints the local calendar summary at the previously selected index.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_WEEKS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_PRINT_WEEKS

plugin calendar-common print weeks

  • Prints the local calendar's weeks.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SELECT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SELECT

plugin calendar-common select [index:1]

  • Selects a calendar to be printed.
    • index - INT8U - The index of the calendar to be selected.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_CAL_INFO

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_CAL_INFO

plugin calendar-common set-cal-info [index:1] [providerId:4] [issuerEventId:4] [calId:4] [startTime:4] [calType:1] [calName:-1] [numberOfSeasons:1] [numberOfWeekProfiles:1] [numberOfDayProfiles:1]

  • Manually set local calendar information.
    • index - INT8U
    • providerId - INT32U
    • issuerEventId - INT32U
    • calId - INT32U
    • startTime - INT32U
    • calType - INT8U
    • calName - OCTET_STRING
    • numberOfSeasons - INT8U
    • numberOfWeekProfiles - INT8U
    • numberOfDayProfiles - INT8U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_DAY_PROF_INFO

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_DAY_PROF_INFO

plugin calendar-common set-day-prof-info [index:1] [dayId:1] [entryId:1] [minutesFromMidnight:2] [data:1]

  • Manually set local calendar's day profiles information.
    • index - INT8U
    • dayId - INT8U
    • entryId - INT8U
    • minutesFromMidnight - INT16U
    • data - INT8U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_SEASONS_INFO

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_SEASONS_INFO

plugin calendar-common set-seasons-info [index:1] [weekId:1] [startDate:4] [weekIdRef:1]

  • Manually set local calendar's seasons information.
    • index - INT8U
    • weekId - INT8U
    • startDate - DATE
    • weekIdRef - INT8U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_WEEK_PROF_INFO

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_SET_WEEK_PROF_INFO

plugin calendar-common set-week-prof-info [index:1] [weekId:1] [dayIdRefMon:1] [dayIdRefTue:1] [dayIdRefWed:1] [dayIdRefThu:1] [dayIdRefFri:1] [dayIdRefSat:1] [dayIdRefSun:1]

  • Manually set local calendar's week profiles information.
    • index - INT8U
    • weekId - INT8U
    • dayIdRefMon - INT8U
    • dayIdRefTue - INT8U
    • dayIdRefWed - INT8U
    • dayIdRefThu - INT8U
    • dayIdRefFri - INT8U
    • dayIdRefSat - INT8U
    • dayIdRefSun - INT8U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_TEST_INIT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_COMMON_PLUGIN_CALENDAR_COMMON_TEST_INIT

plugin calendar-common test-init

  • Initializes test calendars with dummy data.