A struct containing basic information about an endpoint.

#include < af-types.h >

Data Fields

EmberAfClusterInfo clusters [ EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT ]
EmberAfProfileId profileId
uint16_t deviceId
uint8_t endpoint
uint8_t clusterCount

A struct containing basic information about an endpoint.

Field Documentation

◆ clusterCount

uint8_t EmberAfEndpointInfoStruct::clusterCount

◆ clusters

EmberAfClusterInfo EmberAfEndpointInfoStruct::clusters[ EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT ]

◆ deviceId

uint16_t EmberAfEndpointInfoStruct::deviceId

◆ endpoint

uint8_t EmberAfEndpointInfoStruct::endpoint

◆ profileId

EmberAfProfileId EmberAfEndpointInfoStruct::profileId

The documentation for this struct was generated from the following file:
  • af-types.h