#include < af-types.h >

Data Fields

uint32_t requestDateTime
uint32_t implementationDateTime
uint8_t supplyStatus
uint8_t originatorIdSupplyControlBits

Field Documentation

◆ implementationDateTime

uint32_t EmberAfDeviceManagementSupply::implementationDateTime

◆ originatorIdSupplyControlBits

uint8_t EmberAfDeviceManagementSupply::originatorIdSupplyControlBits

◆ requestDateTime

uint32_t EmberAfDeviceManagementSupply::requestDateTime

◆ supplyStatus

uint8_t EmberAfDeviceManagementSupply::supplyStatus

The documentation for this struct was generated from the following file:
  • af-types.h