#include < af-types.h >

Data Fields

uint32_t proposedProviderId
uint32_t implementationDateTime
uint32_t providerChangeControl
uint8_t proposedProviderName [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH +1]
uint8_t proposedProviderContactDetails [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH +1]

Field Documentation

◆ implementationDateTime

uint32_t EmberAfDeviceManagementSupplier::implementationDateTime

◆ proposedProviderContactDetails

uint8_t EmberAfDeviceManagementSupplier::proposedProviderContactDetails[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH +1]

◆ proposedProviderId

uint32_t EmberAfDeviceManagementSupplier::proposedProviderId

◆ proposedProviderName

uint8_t EmberAfDeviceManagementSupplier::proposedProviderName[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH +1]

◆ providerChangeControl

uint32_t EmberAfDeviceManagementSupplier::providerChangeControl

The documentation for this struct was generated from the following file:
  • af-types.h