Plugin Commands: Partner Link Key Exchange
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_ALLOW_PARTNER |
plugin partner-link-key-exchange allow-partner [allowPartner:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PARTNER |
plugin partner-link-key-exchange partner [nodeId:2] [endpoint:1] |
Detailed Description
The partner link key exchange plugin contributes CLI commands to the application framework to be used for controlling facets of link key exchanges among partners.
Macro Definition Documentation
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_ALLOW_PARTNER
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_ALLOW_PARTNER |
plugin partner-link-key-exchange allow-partner [allowPartner:1]
- Set the allow partner flag within the device for Certificate Based Key Exchange
- allowPartner - INT8U - Boolean value to allow or disallow partner based key exchange
◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PARTNER
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PLUGIN_PARTNER_LINK_KEY_EXCHANGE_PARTNER |
plugin partner-link-key-exchange partner [nodeId:2] [endpoint:1]
- Initiate partner link key exchange.
- nodeId - INT16U - The 2 byte short address of the node
- endpoint - INT8U - The endpoint of the device with whom ot start cbke.