EmberAfGbzMessageData Struct Reference
#include <
af-types.h
>
Data Fields |
|
bool | encryption |
uint8_t * | plainPayload |
uint16_t | plainPayloadLength |
uint8_t * | encryptedPayload |
uint16_t | encryptedPayloadLength |
Field Documentation
◆ encryptedPayload
uint8_t* EmberAfGbzMessageData::encryptedPayload |
◆ encryptedPayloadLength
uint16_t EmberAfGbzMessageData::encryptedPayloadLength |
◆ encryption
bool EmberAfGbzMessageData::encryption |
◆ plainPayload
uint8_t* EmberAfGbzMessageData::plainPayload |
◆ plainPayloadLength
uint16_t EmberAfGbzMessageData::plainPayloadLength |
The documentation for this struct was generated from the following file:
-
af-types.h