EmberAfAttributeMetadata Struct Reference
Each attribute has it's metadata stored in such struct.
#include <
af-types.h
>
Data Fields | |
EmberAfAttributeId | attributeId |
EmberAfAttributeType | attributeType |
uint8_t | size |
EmberAfAttributeMask | mask |
EmberAfDefaultOrMinMaxAttributeValue | defaultValue |
Each attribute has it's metadata stored in such struct.
There is only one of these per attribute across all endpoints.
Field Documentation
◆ attributeId
EmberAfAttributeId EmberAfAttributeMetadata::attributeId |
Attribute ID, according to ZCL specs.
◆ attributeType
EmberAfAttributeType EmberAfAttributeMetadata::attributeType |
Attribute type, according to ZCL specs.
◆ defaultValue
EmberAfDefaultOrMinMaxAttributeValue EmberAfAttributeMetadata::defaultValue |
Pointer to the default value union. Actual value stored depends on the mask.
◆ mask
EmberAfAttributeMask EmberAfAttributeMetadata::mask |
Attribute mask, tagging attribute with specific functionality. See ATTRIBUTE_MASK_ macros defined in att-storage.h.
◆ size
uint8_t EmberAfAttributeMetadata::size |
Size of this attribute in bytes.
The documentation for this struct was generated from the following file:
af-types.h