#include < af-types.h >

Data Fields

uint8_t password [ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH +1]
uint32_t implementationDateTime
uint16_t durationInMinutes
EmberAfDeviceManagementPasswordType passwordType

Field Documentation

◆ durationInMinutes

uint16_t EmberAfDeviceManagementPassword::durationInMinutes

◆ implementationDateTime

uint32_t EmberAfDeviceManagementPassword::implementationDateTime

◆ password

uint8_t EmberAfDeviceManagementPassword::password[ EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH +1]

◆ passwordType

EmberAfDeviceManagementPasswordType EmberAfDeviceManagementPassword::passwordType

The documentation for this struct was generated from the following file:
  • af-types.h