Cluster Commands: Level Control

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL
zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE
zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP
zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP
zcl level-control stop [optionMask:1] [optionOverride:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL
zcl level-control o-mv-to-level [level:1] [transitionTime:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE
zcl level-control o-move [moveMode:1] [rate:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP
zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP
zcl level-control o-stop

Detailed Description

This group describes the CLI commands for the Level Control cluster. Listed below is a description of the cluster:

Attributes and commands for controlling devices that can be set to a level between fully 'On' and fully 'Off.'

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MOVE

zcl level-control move [moveMode:1] [rate:1] [optionMask:1] [optionOverride:1]

  • Command description for Move
    • moveMode - MoveMode [ENUM8]
    • rate - INT8U
    • optionMask - BITMAP8
    • optionOverride - BITMAP8
      See also
      EmberAfMoveMode

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_MV_TO_LEVEL

zcl level-control mv-to-level [level:1] [transitionTime:2] [optionMask:1] [optionOverride:1]

  • Command description for MoveToLevel
    • level - INT8U
    • transitionTime - INT16U
    • optionMask - BITMAP8
    • optionOverride - BITMAP8

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MOVE

zcl level-control o-move [moveMode:1] [rate:1]

  • Command description for MoveWithOnOff

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_MV_TO_LEVEL

zcl level-control o-mv-to-level [level:1] [transitionTime:2]

  • Command description for MoveToLevelWithOnOff
    • level - INT8U
    • transitionTime - INT16U

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STEP

zcl level-control o-step [stepMode:1] [stepSize:1] [transitionTime:2]

  • Command description for StepWithOnOff
    • stepMode - StepMode [ENUM8]
    • stepSize - INT8U
    • transitionTime - INT16U
      See also
      EmberAfStepMode

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_O_STOP

zcl level-control o-stop

  • Command description for StopWithOnOff

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STEP

zcl level-control step [stepMode:1] [stepSize:1] [transitionTime:2] [optionMask:1] [optionOverride:1]

  • Command description for Step
    • stepMode - StepMode [ENUM8]
    • stepSize - INT8U
    • transitionTime - INT16U
    • optionMask - BITMAP8
    • optionOverride - BITMAP8
      See also
      EmberAfStepMode

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_LEVEL_CONTROL_STOP

zcl level-control stop [optionMask:1] [optionOverride:1]

  • Command description for Stop
    • optionMask - BITMAP8
    • optionOverride - BITMAP8