Functions

void halRadioPowerUpHandler (void)
Called whenever the radio is powered on.
void halRadioPowerDownHandler (void)
Called whenever the radio is powered off.
void halSleepCallback (boolean enter, SleepModes sleepMode)
Called whenever the microcontroller enters/exits a idle/sleep mode.

Detailed Description

These callbacks are contributed by the HAL Library plugin.

Function Documentation

◆ halRadioPowerDownHandler()

void halRadioPowerDownHandler ( void )

Called whenever the radio is powered off.

◆ halRadioPowerUpHandler()

void halRadioPowerUpHandler ( void )

Called whenever the radio is powered on.

◆ halSleepCallback()

void halSleepCallback ( boolean enter,
SleepModes sleepMode
)

Called whenever the microcontroller enters/exits a idle/sleep mode.

Parameters
enter True if entering idle/sleep, False if exiting
sleepMode Idle/sleep mode