EmberAfClusterList Struct Reference
A list of clusters received during a service discovery attempt. This will be returned for a simple descriptor request.
#include <
af-types.h
>
Data Fields | |
uint8_t | inClusterCount |
const uint16_t * | inClusterList |
uint8_t | outClusterCount |
const uint16_t * | outClusterList |
EmberAfProfileId | profileId |
uint16_t | deviceId |
uint8_t | endpoint |
A list of clusters received during a service discovery attempt. This will be returned for a simple descriptor request.
Field Documentation
◆ deviceId
uint16_t EmberAfClusterList::deviceId |
◆ endpoint
uint8_t EmberAfClusterList::endpoint |
◆ inClusterCount
uint8_t EmberAfClusterList::inClusterCount |
◆ inClusterList
const uint16_t* EmberAfClusterList::inClusterList |
◆ outClusterCount
uint8_t EmberAfClusterList::outClusterCount |
◆ outClusterList
const uint16_t* EmberAfClusterList::outClusterList |
◆ profileId
EmberAfProfileId EmberAfClusterList::profileId |
The documentation for this struct was generated from the following file:
af-types.h