Plugin Commands: Sleepy Message Queue

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_NUM_MSG
plugin sleepy-message-queue getNumMsg [dstEui64:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG
plugin sleepy-message-queue getPendingMsg [msgId:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG_ID
plugin sleepy-message-queue getPendingMsgId [dstEui64:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_INIT
plugin sleepy-message-queue init
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMAIN_TIME
plugin sleepy-message-queue remainTime [msgId:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE
plugin sleepy-message-queue remove [msgId:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE_ALL
plugin sleepy-message-queue removeAll [dstEui64:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_STORE
plugin sleepy-message-queue store [timeoutSec:4] [payloadPtr:4] [payloadLength:2] [payloadId:2] [dstEui64:-1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_TIMESTAMP
plugin sleepy-message-queue timestamp
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_UNUSED_CNT
plugin sleepy-message-queue unusedCnt

Detailed Description

The sleepy-message-queue plugin provides a means to store packets up to a specified period of time.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_NUM_MSG

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_NUM_MSG

plugin sleepy-message-queue getNumMsg [dstEui64:-1]

  • Get the number of pending messages for a given destination EUI64.
    • dstEui64 - OCTET_STRING - The EUI64 of the device for which the number of pending messages is being queried

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG

plugin sleepy-message-queue getPendingMsg [msgId:1]

  • Get the first pending message ID for a given destination EUI64.
    • msgId - INT8U - The messageID of the message to be retrieved.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG_ID

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_GET_PENDING_MSG_ID

plugin sleepy-message-queue getPendingMsgId [dstEui64:-1]

  • Get the first pending message ID for a given destination EUI64.
    • dstEui64 - OCTET_STRING - The EUI64 of the device for which the first pending message ID is being queried

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_INIT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_INIT

plugin sleepy-message-queue init

  • Initialize the sleepy message queue.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMAIN_TIME

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMAIN_TIME

plugin sleepy-message-queue remainTime [msgId:1]

  • Report the remaining timeout on the message specified by the message ID.
    • msgId - INT8U - The messageID of the message whose remaining time will be reported.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE

plugin sleepy-message-queue remove [msgId:1]

  • Remove the message from the queue with the given messageID.
    • msgId - INT8U - The messageID of the message to be removed.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE_ALL

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_REMOVE_ALL

plugin sleepy-message-queue removeAll [dstEui64:-1]

  • Remove all messages from the queue with the given EUI64.
    • dstEui64 - OCTET_STRING - The EUI64 of the device whose messages should be removed.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_STORE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_STORE

plugin sleepy-message-queue store [timeoutSec:4] [payloadPtr:4] [payloadLength:2] [payloadId:2] [dstEui64:-1]

  • Store a message into the sleepy message queue.
    • timeoutSec - INT32U - Message timeout, in seconds
    • payloadPtr - INT32U - Pointer to (address of) the message payload
    • payloadLength - INT16U - The length of the message payload
    • payloadId - INT16U - The payload ID of this message
    • dstEui64 - OCTET_STRING - The EUI64 of the device to which the message is being sent

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_TIMESTAMP

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_TIMESTAMP

plugin sleepy-message-queue timestamp

  • Retrieve the current value of halCommonGetInt32uMillisecondTick().

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_UNUSED_CNT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLEEPY_MESSAGE_QUEUE_PLUGIN_SLEEPY_MESSAGE_QUEUE_UNUSED_CNT

plugin sleepy-message-queue unusedCnt

  • Reads the number of unused queue entries.