EmberAfAllowedInterPanMessage Struct Reference
This structure is used define an interpan message that will be accepted by the interpan filters.
#include <
af-types.h
>
Data Fields | |
EmberAfProfileId | profileId |
EmberAfClusterId | clusterId |
uint8_t | commandId |
EmberAfAllowedInterpanOptions | options |
This structure is used define an interpan message that will be accepted by the interpan filters.
Field Documentation
◆ clusterId
EmberAfClusterId EmberAfAllowedInterPanMessage::clusterId |
◆ commandId
uint8_t EmberAfAllowedInterPanMessage::commandId |
◆ options
EmberAfAllowedInterpanOptions EmberAfAllowedInterPanMessage::options |
◆ profileId
EmberAfProfileId EmberAfAllowedInterPanMessage::profileId |
The documentation for this struct was generated from the following file:
af-types.h