EmberAfIncomingMessage Struct Reference
a struct containing the superset of values passed to both emberIncomingMessageHandler on the SOC and ezspIncomingMessageHandler on the host.
#include <
af-types.h
>
Data Fields |
|
EmberIncomingMessageType | type |
EmberApsFrame * | apsFrame |
uint8_t * | message |
uint16_t | msgLen |
uint16_t | source |
uint8_t | lastHopLqi |
int8_t | lastHopRssi |
uint8_t | bindingTableIndex |
uint8_t | addressTableIndex |
uint8_t | networkIndex |
a struct containing the superset of values passed to both emberIncomingMessageHandler on the SOC and ezspIncomingMessageHandler on the host.
Field Documentation
◆ addressTableIndex
uint8_t EmberAfIncomingMessage::addressTableIndex |
The index of the entry in the address table that matches the sender of the message or 0xFF if there is no matching entry.
◆ apsFrame
EmberApsFrame * EmberAfIncomingMessage::apsFrame |
APS frame for the incoming message
◆ bindingTableIndex
uint8_t EmberAfIncomingMessage::bindingTableIndex |
The index of a binding that matches the message or 0xFF if there is no matching binding.
◆ lastHopLqi
uint8_t EmberAfIncomingMessage::lastHopLqi |
Link quality from the node that last relayed the message.
◆ lastHopRssi
int8_t EmberAfIncomingMessage::lastHopRssi |
The energy level (in units of dBm) observed during the reception.
◆ message
uint8_t* EmberAfIncomingMessage::message |
The message copied into a flat buffer
◆ msgLen
uint16_t EmberAfIncomingMessage::msgLen |
Length of the incoming message
◆ networkIndex
uint8_t EmberAfIncomingMessage::networkIndex |
The index of the network on which this message was received.
◆ source
uint16_t EmberAfIncomingMessage::source |
Two byte node id of the sending node.
◆ type
EmberIncomingMessageType EmberAfIncomingMessage::type |
The type of the incoming message
The documentation for this struct was generated from the following file:
-
af-types.h