Functions

void emberAfPluginMicriumRtosAppTask1InitCallback (void)
This function is called from the Micrium RTOS plugin before the Application (1) task is created.
void emberAfPluginMicriumRtosAppTask1MainLoopCallback (void *p_arg)
This function implements the Application (1) task main loop.
void emberAfPluginMicriumRtosAppTask2InitCallback (void)
This function is called from the Micrium RTOS plugin before the Application (2) task is created.
void emberAfPluginMicriumRtosAppTask2MainLoopCallback (void *p_arg)
This function implements the Application (2) task main loop.
void emberAfPluginMicriumRtosAppTask3InitCallback (void)
This function is called from the Micrium RTOS plugin before the Application (3) task is created.
void emberAfPluginMicriumRtosAppTask3MainLoopCallback (void *p_arg)
This function implements the Application (3) task main loop.

Detailed Description

These callbacks are contributed by the Micrium RTOS plugin.

Function Documentation

◆ emberAfPluginMicriumRtosAppTask1InitCallback()

void emberAfPluginMicriumRtosAppTask1InitCallback ( void )

This function is called from the Micrium RTOS plugin before the Application (1) task is created.

◆ emberAfPluginMicriumRtosAppTask1MainLoopCallback()

void emberAfPluginMicriumRtosAppTask1MainLoopCallback ( void * p_arg )

This function implements the Application (1) task main loop.

Parameters
p_arg Ver.: always

◆ emberAfPluginMicriumRtosAppTask2InitCallback()

void emberAfPluginMicriumRtosAppTask2InitCallback ( void )

This function is called from the Micrium RTOS plugin before the Application (2) task is created.

◆ emberAfPluginMicriumRtosAppTask2MainLoopCallback()

void emberAfPluginMicriumRtosAppTask2MainLoopCallback ( void * p_arg )

This function implements the Application (2) task main loop.

Parameters
p_arg Ver.: always

◆ emberAfPluginMicriumRtosAppTask3InitCallback()

void emberAfPluginMicriumRtosAppTask3InitCallback ( void )

This function is called from the Micrium RTOS plugin before the Application (3) task is created.

◆ emberAfPluginMicriumRtosAppTask3MainLoopCallback()

void emberAfPluginMicriumRtosAppTask3MainLoopCallback ( void * p_arg )

This function implements the Application (3) task main loop.

Parameters
p_arg Ver.: always