A data struct used to keep track of incoming and outgoing commands for command discovery.

#include < af-types.h >

Data Fields

uint16_t clusterId
uint8_t commandId
uint8_t mask

A data struct used to keep track of incoming and outgoing commands for command discovery.

Field Documentation

◆ clusterId

uint16_t EmberAfCommandMetadata::clusterId

◆ commandId

uint8_t EmberAfCommandMetadata::commandId

◆ mask

uint8_t EmberAfCommandMetadata::mask

The documentation for this struct was generated from the following file:
  • af-types.h