EmberNetworkParameters Struct Reference
Holds network parameters.
#include <
ember-types.h
>
Data Fields | |
uint8_t | extendedPanId [EXTENDED_PAN_ID_SIZE] |
uint16_t | panId |
int8_t | radioTxPower |
uint8_t | radioChannel |
EmberJoinMethod | joinMethod |
EmberNodeId | nwkManagerId |
uint8_t | nwkUpdateId |
uint32_t | channels |
Holds network parameters.
For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit.
Field Documentation
◆ channels
uint32_t EmberNetworkParameters::channels |
The NWK channel mask. The list of preferred channels that the NWK manager has told this device to use when searching for the network. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.
◆ extendedPanId
uint8_t EmberNetworkParameters::extendedPanId[EXTENDED_PAN_ID_SIZE] |
The network's extended PAN identifier.
Referenced by initNetworkParams()
.
◆ joinMethod
EmberJoinMethod EmberNetworkParameters::joinMethod |
Join method: The protocol messages used to establish an initial parent. It is ignored when forming a ZigBee network, or when querying the stack for its network parameters.
◆ nwkManagerId
EmberNodeId EmberNetworkParameters::nwkManagerId |
NWK Manager ID. The ID of the network manager in the current network. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.
◆ nwkUpdateId
uint8_t EmberNetworkParameters::nwkUpdateId |
An NWK Update ID. The value of the ZigBee nwkUpdateId known by the stack. It is used to determine the newest instance of the network after a PAN ID or channel change. This may only be set at joining when using EMBER_USE_CONFIGURED_NWK_STATE as the join method.
◆ panId
uint16_t EmberNetworkParameters::panId |
The network's PAN identifier.
Referenced by initNetworkParams()
.
◆ radioChannel
uint8_t EmberNetworkParameters::radioChannel |
A radio channel. Be sure to specify a channel supported by the radio.
Referenced by initNetworkParams()
.
◆ radioTxPower
int8_t EmberNetworkParameters::radioTxPower |
A power setting, in dBm.
Referenced by initNetworkParams()
.
The documentation for this struct was generated from the following file:
ember-types.h