Union describing the attribute default/min/max values.

#include < af-types.h >

Data Fields

uint8_t * ptrToDefaultValue
uint16_t defaultValue
EmberAfAttributeMinMaxValue * ptrToMinMaxValue

Union describing the attribute default/min/max values.

Field Documentation

◆ defaultValue

uint16_t EmberAfDefaultOrMinMaxAttributeValue::defaultValue

Actual default value if the attribute size is 2 bytes or less.

◆ ptrToDefaultValue

uint8_t* EmberAfDefaultOrMinMaxAttributeValue::ptrToDefaultValue

Points to data if size is more than 2 bytes. If size is more than 2 bytes, and this value is NULL, then the default value is all zeroes.

◆ ptrToMinMaxValue

EmberAfAttributeMinMaxValue * EmberAfDefaultOrMinMaxAttributeValue::ptrToMinMaxValue

Points to the min max attribute value structure, if min/max is supported for this attribute.


The documentation for this union was generated from the following file:
  • af-types.h