Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_ADD
plugin reporting add [endpoint:1] [clusterId:2] [attributeId:2] [mask:1] [minInterval:2] [maxInterval:2] [reportableChange:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR
plugin reporting clear
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR_LAST_REPORT_TIME
plugin reporting clear-last-report-time
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_PRINT
plugin reporting print
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_REMOVE
plugin reporting remove [index:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_TEST_TIMING
plugin reporting test-timing

Detailed Description

The reporting plugin contributes several CLI commands to the application framework to be used in creating and managing reporting table entries directly on the device.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_ADD

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_ADD

plugin reporting add [endpoint:1] [clusterId:2] [attributeId:2] [mask:1] [minInterval:2] [maxInterval:2] [reportableChange:4]

  • Add a new entry to the report table.
    • endpoint - INT8U - The local endpoint from which the attribute is reported.
    • clusterId - INT16U - The cluster where the attribute is located.
    • attributeId - INT16U - The id of the attribute being reported.
    • mask - INT8U - 0 for client-side attributes or 1 for server-side attributes.
    • minInterval - INT16U - The minimum reporting interval, measured in seconds.
    • maxInterval - INT16U - The maximum reporting interval, measured in seconds.
    • reportableChange - INT32U - The minimum change to the attribute that will result in a report being sent.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR

plugin reporting clear

  • Clear all entries from the report table.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR_LAST_REPORT_TIME

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR_LAST_REPORT_TIME

plugin reporting clear-last-report-time

  • Clear last report time of attributes.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_PRINT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_PRINT

plugin reporting print

  • Print the report table.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_REMOVE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_REMOVE

plugin reporting remove [index:1]

  • Remove an entry from the report table.
    • index - INT8U - The index of the report to be removed.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_TEST_TIMING

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_TEST_TIMING

plugin reporting test-timing

  • FOR TESTING PURPOSES - gather timing metrics for reporting table operations