Plugin Commands: Meter Snapshot Server

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_PUBLISH
plugin meter-snapshot-server publish [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [startTime:4] [endTime:4] [offset:1] [cause:4]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_TAKE
plugin meter-snapshot-server take [endpoint:1] [cause:4]

Detailed Description

The meter-snapshot-server plugin contributes several commands to the application framework's CLI. These commands are used for taking and publishing snapshots.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_PUBLISH

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_PUBLISH

plugin meter-snapshot-server publish [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [startTime:4] [endTime:4] [offset:1] [cause:4]

  • Publish a snapshot.
    • nodeId - INT16U - the destination node id
    • srcEndpoint - INT8U - the source endpoint
    • dstEndpoint - INT8U - the destination endpoint
    • startTime - INT32U - the earliest time of a snapshot to be published
    • endTime - INT32U - the latest time of a snapshot to be published
    • offset - INT8U - identifies the snapshot to be published
    • cause - INT32U - select only snapshots that were taken due to a specific cause

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_TAKE

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_TAKE

plugin meter-snapshot-server take [endpoint:1] [cause:4]

  • Take a snapshot.
    • endpoint - INT8U - the source endpoint
    • cause - INT32U - the cause of the snapshot