Plugin Commands: Calendar Client

Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_CLEAR
plugin calendar-client clear [endpoint:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_PRINT
plugin calendar-client print [endpoint:1]

Detailed Description

The Calendar Client plugin contributes several commands to the application framework's CLI. These commands are used for interacting with calendars.

Macro Definition Documentation

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_CLEAR

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_CLEAR

plugin calendar-client clear [endpoint:1]

  • Clear the calendars.
    • endpoint - INT8U - The endpoint.

◆ EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_PRINT

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_PRINT

plugin calendar-client print [endpoint:1]

  • Print the calendars.
    • endpoint - INT8U - The endpoint.