Functions

void coexCoulombCounterEventCallback (uint16_t ccState)
Reports a change in radio state.

Detailed Description

These callbacks are contributed by the Radio Coexistence plugin.

Function Documentation

◆ coexCoulombCounterEventCallback()

void coexCoulombCounterEventCallback ( uint16_t ccState )

Reports a change in radio state.

This function is called by the RAIL library to report changes in the radio states (Idle/Rx/Tx) according to PTA events.

Parameters
ccState bitmask of radio states