This structure contains information about a tag that resides within an Over-the-air bootload file.

#include < af-types.h >

Data Fields

uint16_t id
uint32_t length

This structure contains information about a tag that resides within an Over-the-air bootload file.

Field Documentation

◆ id

uint16_t EmberAfTagData::id

◆ length

uint32_t EmberAfTagData::length

The documentation for this struct was generated from the following file:
  • af-types.h