Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SET
zcl tstat set [mode:1] [amount:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SWS
zcl tstat sws [numberOfTransitionsForSequence:1] [dayOfWeekForSequence:1] [modeForSequence:1] [payload:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GWS
zcl tstat gws [daysToReturn:1] [modeToReturn:1]
#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_CWS
zcl tstat cws
#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GRS
zcl tstat grs

Detailed Description

This group describes the CLI commands for the Thermostat cluster. Listed below is a description of the cluster:

An interface for configuring and controlling the functionality of a thermostat.

Macro Definition Documentation

EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_CWS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_CWS

zcl tstat cws

  • The Clear Weekly Schedule command is used to clear the weekly schedule.

EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GRS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GRS

zcl tstat grs

  • The Get Relay Status Log command is used to query the thermostat internal relay status log.

EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GWS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_GWS

zcl tstat gws [daysToReturn:1] [modeToReturn:1]

  • Command description for GetWeeklySchedule
    • daysToReturn - DayOfWeek [BITMAP8]
    • modeToReturn - ModeForSequence [BITMAP8]

EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SET

#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SET

zcl tstat set [mode:1] [amount:1]

EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SWS

#define EMBER_AF_DOXYGEN_CLI_COMMAND_THERMOSTAT_SWS

zcl tstat sws [numberOfTransitionsForSequence:1] [dayOfWeekForSequence:1] [modeForSequence:1] [payload:1]

  • Command description for SetWeeklySchedule
    • numberOfTransitionsForSequence - ENUM8
    • dayOfWeekForSequence - DayOfWeek [BITMAP8]
    • modeForSequence - ModeForSequence [BITMAP8]
    • payload - INT8U