Zigbee Internet Client/Server Remote Binding struct.

#include < af-types.h >

Data Fields

EmberEUI64 targetEUI64
uint8_t sourceEndpoint
uint8_t destEndpoint
uint16_t clusterId
EmberEUI64 destEUI64
EmberEUI64 sourceEUI64

Zigbee Internet Client/Server Remote Binding struct.

Field Documentation

◆ clusterId

uint16_t EmberAfRemoteBindingStruct::clusterId

◆ destEndpoint

uint8_t EmberAfRemoteBindingStruct::destEndpoint

◆ destEUI64

EmberEUI64 EmberAfRemoteBindingStruct::destEUI64

◆ sourceEndpoint

uint8_t EmberAfRemoteBindingStruct::sourceEndpoint

◆ sourceEUI64

EmberEUI64 EmberAfRemoteBindingStruct::sourceEUI64

◆ targetEUI64

EmberEUI64 EmberAfRemoteBindingStruct::targetEUI64

The documentation for this struct was generated from the following file:
  • af-types.h