Zigbee Internet Client/Server remote cluster struct.

#include < af-types.h >

Data Fields

EmberAfClusterId clusterId
EmberAfProfileId profileId
uint16_t deviceId
uint8_t endpoint
EmberAfRemoteClusterType type

Zigbee Internet Client/Server remote cluster struct.

Field Documentation

◆ clusterId

EmberAfClusterId EmberAfRemoteClusterStruct::clusterId

◆ deviceId

uint16_t EmberAfRemoteClusterStruct::deviceId

◆ endpoint

uint8_t EmberAfRemoteClusterStruct::endpoint

◆ profileId

EmberAfProfileId EmberAfRemoteClusterStruct::profileId

◆ type

EmberAfRemoteClusterType EmberAfRemoteClusterStruct::type

The documentation for this struct was generated from the following file:
  • af-types.h