IADCEMLIB
Detailed Description
Incremental Analog to Digital Converter (IADC) Peripheral API.
This module contains functions to control the IADC peripheral of Silicon Labs 32-bit MCUs and SoCs. The IADC is used to convert analog signals into a digital representation.
         Data Structures | 
       |
| struct | IADC_AllConfigs_t | 
| struct | IADC_Config_t | 
| struct | IADC_Init_t | 
| struct | IADC_InitScan_t | 
| struct | IADC_InitSingle_t | 
| struct | IADC_Result_t | 
| struct | IADC_ScanTable_t | 
| struct | IADC_ScanTableEntry_t | 
| struct | IADC_SingleInput_t | 
         Macros | 
       |
| #define | IADC_ALLCONFIGS_DEFAULT | 
| #define | IADC_CONFIG_DEFAULT | 
| #define | IADC_INIT_DEFAULT | 
| #define | IADC_INITSCAN_DEFAULT | 
| #define | IADC_INITSINGLE_DEFAULT | 
| #define | IADC_SCANTABLE_DEFAULT | 
| #define | IADC_SCANTABLEENTRY_DEFAULT | 
| #define | IADC_SINGLEINPUT_DEFAULT | 
         Functions | 
       |
| uint8_t | IADC_calcAdcClkPrescale ( IADC_TypeDef *iadc, uint32_t adcClkFreq, uint32_t cmuClkFreq, IADC_CfgAdcMode_t adcMode, uint8_t srcClkPrescaler) | 
| 
         Calculate prescaler for ADC_CLK clock.
          | 
       |
| uint8_t | IADC_calcSrcClkPrescale ( IADC_TypeDef *iadc, uint32_t srcClkFreq, uint32_t cmuClkFreq) | 
| 
         Calculate prescaler for CLK_SRC_ADC high speed clock.
          | 
       |
| uint8_t | IADC_calcTimebase ( IADC_TypeDef *iadc, uint32_t cmuClkFreq) | 
| 
         Calculate timebase value in order to get a timebase providing at least 1us.
          | 
       |
| __STATIC_INLINE void | IADC_clearInt ( IADC_TypeDef *iadc, uint32_t flags) | 
| 
         Clear one or more pending IADC interrupts.
          | 
       |
| __STATIC_INLINE void | IADC_command ( IADC_TypeDef *iadc, IADC_Cmd_t cmd) | 
| 
         Start/stop scan sequence, single conversion and/or timer.
          | 
       |
| __STATIC_INLINE void | IADC_disableInt ( IADC_TypeDef *iadc, uint32_t flags) | 
| 
         Disable one or more IADC interrupts.
          | 
       |
| __STATIC_INLINE void | IADC_enableInt ( IADC_TypeDef *iadc, uint32_t flags) | 
| 
         Enable one or more IADC interrupts.
          | 
       |
| __STATIC_INLINE uint32_t | IADC_getEnabledInt ( IADC_TypeDef *iadc) | 
| 
         Get enabled and pending IADC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
          | 
       |
| __STATIC_INLINE uint32_t | IADC_getInt ( IADC_TypeDef *iadc) | 
| 
         Get pending IADC interrupt flags.
          | 
       |
| __STATIC_INLINE uint8_t | IADC_getScanFifoCnt ( IADC_TypeDef *iadc) | 
| 
         Get number of elements in the IADC scan FIFO.
          | 
       |
| __STATIC_INLINE uint32_t | IADC_getScanMask ( IADC_TypeDef *iadc) | 
| 
         Get the scan mask currently used in the IADC.
          | 
       |
| __STATIC_INLINE uint8_t | IADC_getSingleFifoCnt ( IADC_TypeDef *iadc) | 
| 
         Get number of elements in the IADC single FIFO.
          | 
       |
| __STATIC_INLINE uint32_t | IADC_getStatus ( IADC_TypeDef *iadc) | 
| 
         Get status bits of IADC.
          | 
       |
| void | IADC_init ( IADC_TypeDef *iadc, const IADC_Init_t *init, const IADC_AllConfigs_t *allConfigs) | 
| 
         Initialize IADC.
          | 
       |
| void | IADC_initScan ( IADC_TypeDef *iadc, const IADC_InitScan_t *init, const IADC_ScanTable_t *scanTable) | 
| 
         Initialize IADC scan sequence.
          | 
       |
| void | IADC_initSingle ( IADC_TypeDef *iadc, const IADC_InitSingle_t *init, const IADC_SingleInput_t *input) | 
| 
         Initialize single IADC conversion.
          | 
       |
| __STATIC_INLINE IADC_NegInput_t | IADC_portPinToNegInput ( GPIO_Port_TypeDef port, uint8_t pin) | 
| 
         Convert GPIO port/pin to IADC negative input selection.
          | 
       |
| __STATIC_INLINE IADC_PosInput_t | IADC_portPinToPosInput ( GPIO_Port_TypeDef port, uint8_t pin) | 
| 
         Convert GPIO port/pin to IADC positive input selection.
          | 
       |
| __STATIC_INLINE uint32_t | IADC_pullScanFifoData ( IADC_TypeDef *iadc) | 
| 
         Pull data from scan data FIFO. If showId was set for the scan entry initialization, the data will contain the ID of the scan entry.
          | 
       |
| IADC_Result_t | IADC_pullScanFifoResult ( IADC_TypeDef *iadc) | 
| 
         Pull result from scan data FIFO. The result struct includes both the data and the ID (0x20) if showId was set when initializing scan entry.
          | 
       |
| __STATIC_INLINE uint32_t | IADC_pullSingleFifoData ( IADC_TypeDef *iadc) | 
| 
         Pull data from single data FIFO. If showId was set when initializing single mode, the results will contain the ID (0x20).
          | 
       |
| IADC_Result_t | IADC_pullSingleFifoResult ( IADC_TypeDef *iadc) | 
| 
         Pull result from single data FIFO. The result struct includes both the data and the ID (0x20) if showId was set when initializing single mode.
          | 
       |
| __STATIC_INLINE uint32_t | IADC_readScanData ( IADC_TypeDef *iadc) | 
| 
         Read most recent scan conversion data. If showId was set for the scan entry initialization, the data will contain the ID of the scan entry. Calling this function will not affect the state of the scan data FIFO.
          | 
       |
| IADC_Result_t | IADC_readScanResult ( IADC_TypeDef *iadc) | 
| 
         Read most recent scan conversion result. The result struct includes both the data and the ID (0x20) if showId was set when initializing scan entry. Calling this function will not affect the state of the scan data FIFO.
          | 
       |
| __STATIC_INLINE uint32_t | IADC_readSingleData ( IADC_TypeDef *iadc) | 
| 
         Read most recent single conversion data. If showId was set when initializing single mode, the data will contain the ID (0x20). Calling this function will not affect the state of the single data FIFO.
          | 
       |
| IADC_Result_t | IADC_readSingleResult ( IADC_TypeDef *iadc) | 
| 
         Read most recent single conversion result. The result struct includes both the data and the ID (0x20) if showId was set when initializing single mode. Calling this function will not affect the state of the single data FIFO.
          | 
       |
| void | IADC_reset ( IADC_TypeDef *iadc) | 
| 
         Reset IADC to same state as after a HW reset.
          | 
       |
| __STATIC_INLINE void | IADC_setInt ( IADC_TypeDef *iadc, uint32_t flags) | 
| 
         Set one or more pending IADC interrupts from SW.
          | 
       |
| void | IADC_setScanMask ( IADC_TypeDef *iadc, uint32_t mask) | 
| 
         Set mask of IADC scan table entries to include in scan.
          | 
       |
| void | IADC_updateScanEntry ( IADC_TypeDef *iadc, uint8_t id, IADC_ScanTableEntry_t *entry) | 
| 
         Add/update entry in scan table.
          | 
       |
| void | IADC_updateSingleInput ( IADC_TypeDef *iadc, const IADC_SingleInput_t *input) | 
| 
         Update IADC single input selection.
          | 
       |
Macro Definition Documentation
| #define IADC_ALLCONFIGS_DEFAULT | 
Default IADC sructure for all configs.
        Definition at line
        
         690
        
        of file
        
         em_iadc.h
        
        .
       
| #define IADC_CONFIG_DEFAULT | 
Default IADC config structure.
        Definition at line
        
         672
        
        of file
        
         em_iadc.h
        
        .
       
| #define IADC_INIT_DEFAULT | 
Default config for IADC init structure.
        Definition at line
        
         647
        
        of file
        
         em_iadc.h
        
        .
       
| #define IADC_INITSCAN_DEFAULT | 
Default config for IADC scan init structure.
        Definition at line
        
         710
        
        of file
        
         em_iadc.h
        
        .
       
| #define IADC_INITSINGLE_DEFAULT | 
Default config for IADC single init structure.
        Definition at line
        
         735
        
        of file
        
         em_iadc.h
        
        .
       
| #define IADC_SCANTABLE_DEFAULT | 
Default IADC sructure for scan table
        Definition at line
        
         790
        
        of file
        
         em_iadc.h
        
        .
       
| #define IADC_SCANTABLEENTRY_DEFAULT | 
Default config for IADC scan table entry structure.
        Definition at line
        
         774
        
        of file
        
         em_iadc.h
        
        .
       
| #define IADC_SINGLEINPUT_DEFAULT | 
Default config for IADC single input structure.
        Definition at line
        
         756
        
        of file
        
         em_iadc.h
        
        .
       
Enumeration Type Documentation
| enum IADC_Alignment_t | 
| enum IADC_CfgAdcMode_t | 
| enum IADC_CfgAnalogGain_t | 
IADC Over sampling rate for high speed.
        Definition at line
        
         535
        
        of file
        
         em_iadc.h
        
        .
       
| enum IADC_CfgReference_t | 
IADC Reference
        Definition at line
        
         571
        
        of file
        
         em_iadc.h
        
        .
       
| enum IADC_CfgTwosComp_t | 
IADC Two's complement results
        Definition at line
        
         586
        
        of file
        
         em_iadc.h
        
        .
       
| enum IADC_Cmd_t | 
| enum IADC_NegInput_t | 
IADC negative input selection.
        Definition at line
        
         82
        
        of file
        
         em_iadc.h
        
        .
       
| enum IADC_PosInput_t | 
IADC positive port selection.
        Definition at line
        
         283
        
        of file
        
         em_iadc.h
        
        .
       
| enum IADC_TriggerAction_t | 
| enum IADC_TriggerSel_t | 
IADC trigger action
        Definition at line
        
         598
        
        of file
        
         em_iadc.h
        
        .
       
| enum IADC_Warmup_t | 
Function Documentation
| uint8_t IADC_calcAdcClkPrescale | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint32_t | 
           
            adcClkFreq,
           
           | 
         ||
| uint32_t | 
           
            cmuClkFreq,
           
           | 
         ||
| IADC_CfgAdcMode_t | 
           
            adcMode,
           
           | 
         ||
| uint8_t | 
           
            srcClkPrescaler
           
           | 
         ||
| ) | 
Calculate prescaler for ADC_CLK clock.
The ADC_CLK is given by: CLK_SRC_ADC / (adcClkprescale + 1).
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] adcClkFreqADC_CLK frequency wanted. The frequency will automatically be adjusted to be within valid range according to reference manual. [in] CmuClkFreqFrequency in Hz of CLK_CMU_ADC Set to 0 to use currently defined IADC clock setting (in CMU). [in] adcModeMode for IADC config. [in] srcClkPrescalerPrecaler setting for ADC_CLK  
- Returns
 - 
         Divider value to use for IADC in order to achieve a ADC_CLK frequency <=
         
adcClkFreq. 
        Definition at line
        
         807
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_SCHED_PRESCALE_MASK , _IADC_SCHED_PRESCALE_SHIFT , CMU_ClockFreqGet() , and SL_MIN .
Referenced by IADC_init() .
| uint8_t IADC_calcSrcClkPrescale | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint32_t | 
           
            srcClkFreq,
           
           | 
         ||
| uint32_t | 
           
            cmuClkFreq
           
           | 
         ||
| ) | 
Calculate prescaler for CLK_SRC_ADC high speed clock.
The IADC high speed clock is given by: CLK_SRC_ADC / (srcClkPrescaler + 1).
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] srcClkFreqCLK_SRC_ADC frequency wanted. The frequency will automatically be adjusted to be within valid range according to reference manual. [in] cmuClkFreqFrequency in Hz of reference CLK_CMU_ADC. Set to 0 to use currently defined CMU clock setting for the IADC.  
- Returns
 - 
         Divider value to use for IADC in order to achieve a high speed clock value <=
         
srcClkFreq. 
        Definition at line
        
         753
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_CTRL_HSCLKRATE_DIV4 , CMU_ClockFreqGet() , and SL_MIN .
Referenced by IADC_init() .
| uint8_t IADC_calcTimebase | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint32_t | 
           
            cmuClkFreq
           
           | 
         ||
| ) | 
Calculate timebase value in order to get a timebase providing at least 1us.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] cmuClkFreqFrequency in Hz of reference CLK_CMU_ADC clock. Set to 0 to use currently defined CMU clock setting for the IADC.  
- Returns
 - Timebase value to use for IADC in order to achieve at least 1 us.
 
        Definition at line
        
         706
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_CTRL_TIMEBASE_MASK , _IADC_CTRL_TIMEBASE_SHIFT , CMU_ClockFreqGet() , and SL_MIN .
Referenced by IADC_init() .
| __STATIC_INLINE void IADC_clearInt | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Clear one or more pending IADC interrupts.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] flagsPending IADC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).  
        Definition at line
        
         940
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::IF_CLR .
Referenced by IADC_reset() .
| __STATIC_INLINE void IADC_command | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| IADC_Cmd_t | 
           
            cmd
           
           | 
         ||
| ) | 
Start/stop scan sequence, single conversion and/or timer.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] cmdCommand to be performed.  
        Definition at line
        
         1062
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::CMD .
Referenced by IADC_initScan() , and IADC_initSingle() .
| __STATIC_INLINE void IADC_disableInt | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Disable one or more IADC interrupts.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] flagsIADC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).  
        Definition at line
        
         956
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::IEN , and IADC_TypeDef::IEN_CLR .
Referenced by IADC_reset() .
| __STATIC_INLINE void IADC_enableInt | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Enable one or more IADC interrupts.
- Note
 - Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using IADC_intClear() prior to enabling if such a pending interrupt should be ignored.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] flagsIADC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).  
        Definition at line
        
         981
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::IEN .
| __STATIC_INLINE uint32_t IADC_getEnabledInt | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Get enabled and pending IADC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
 - Interrupt flags are not cleared by the use of this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - 
         Pending and enabled IADC interrupt sources. The return value is the bitwise AND combination of
         
- the OR combination of enabled interrupt sources in IADCx_IEN_nnn register (IADCx_IEN_nnn) and
 - the OR combination of valid interrupt flags of the IADC module (IADCx_IF_nnn).
 
 
        Definition at line
        
         1024
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::IEN , and IADC_TypeDef::IF .
| __STATIC_INLINE uint32_t IADC_getInt | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Get pending IADC interrupt flags.
- Note
 - The event bits are not cleared by the use of this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - IADC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).
 
        Definition at line
        
         1000
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::IF .
| __STATIC_INLINE uint8_t IADC_getScanFifoCnt | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Get number of elements in the IADC scan FIFO.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Number of elements in scan FIFO
 
        Definition at line
        
         1123
        
        of file
        
         em_iadc.h
        
        .
       
References _IADC_SCANFIFOSTAT_FIFOREADCNT_MASK , _IADC_SCANFIFOSTAT_FIFOREADCNT_SHIFT , and IADC_TypeDef::SCANFIFOSTAT .
| __STATIC_INLINE uint32_t IADC_getScanMask | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Get the scan mask currently used in the IADC.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Mask of scan table entries currently included in scan.
 
        Definition at line
        
         1077
        
        of file
        
         em_iadc.h
        
        .
       
References _IADC_STMASK_STMASK_SHIFT , and IADC_TypeDef::STMASK .
| __STATIC_INLINE uint8_t IADC_getSingleFifoCnt | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Get number of elements in the IADC single FIFO.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Number of elements in single FIFO
 
        Definition at line
        
         1107
        
        of file
        
         em_iadc.h
        
        .
       
References _IADC_SINGLEFIFOSTAT_FIFOREADCNT_MASK , _IADC_SINGLEFIFOSTAT_FIFOREADCNT_SHIFT , and IADC_TypeDef::SINGLEFIFOSTAT .
| __STATIC_INLINE uint32_t IADC_getStatus | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Get status bits of IADC.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - IADC status bits
 
        Definition at line
        
         1092
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::STATUS .
| void IADC_init | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| const IADC_Init_t * | 
           
            init,
           
           | 
         ||
| const IADC_AllConfigs_t * | 
           
            allConfigs
           
           | 
         ||
| ) | 
Initialize IADC.
Initializes common parts for both single conversion and scan sequence. In addition, single and/or scan control configuration must be done, please refer to IADC_initSingle() and IADC_initScan() respectively.
- Note
 - This function will stop any ongoing conversions.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] initPointer to IADC initialization structure. [in] allConfigsPointer to structure holding all configs.  
        Definition at line
        
         166
        
        of file
        
         em_iadc.c
        
        .
       
References _DEVINFO_IADC0GAIN0_GAINCANA1_MASK , _DEVINFO_IADC0GAIN0_GAINCANA2_SHIFT , _DEVINFO_IADC0GAIN1_GAINCANA3_MASK , _DEVINFO_IADC0GAIN1_GAINCANA4_SHIFT , _DEVINFO_IADC0NORMALOFFSETCAL0_OFFSETANA1NORM_MASK , _DEVINFO_IADC0NORMALOFFSETCAL0_OFFSETANA2NORM_SHIFT , _DEVINFO_IADC0NORMALOFFSETCAL1_OFFSETANA3NORM_MASK , _DEVINFO_IADC0OFFSETCAL0_OFFSETANABASE_MASK , _IADC_CFG_ADCMODE_MASK , _IADC_CFG_ADCMODE_SHIFT , _IADC_CFG_ANALOGGAIN_ANAGAIN0P5 , _IADC_CFG_ANALOGGAIN_ANAGAIN1 , _IADC_CFG_ANALOGGAIN_ANAGAIN2 , _IADC_CFG_ANALOGGAIN_ANAGAIN3 , _IADC_CFG_ANALOGGAIN_MASK , _IADC_CFG_ANALOGGAIN_SHIFT , _IADC_CFG_OSRHS_MASK , _IADC_CFG_OSRHS_SHIFT , _IADC_CFG_REFSEL_MASK , _IADC_CFG_REFSEL_SHIFT , _IADC_CFG_TWOSCOMPL_MASK , _IADC_CFG_TWOSCOMPL_SHIFT , _IADC_CMPTHR_ADGT_MASK , _IADC_CMPTHR_ADGT_SHIFT , _IADC_CMPTHR_ADLT_MASK , _IADC_CMPTHR_ADLT_SHIFT , _IADC_CTRL_HSCLKRATE_MASK , _IADC_CTRL_HSCLKRATE_SHIFT , _IADC_CTRL_TIMEBASE_MASK , _IADC_CTRL_TIMEBASE_SHIFT , _IADC_CTRL_WARMUPMODE_MASK , _IADC_CTRL_WARMUPMODE_SHIFT , _IADC_SCALE_GAIN13LSB_SHIFT , _IADC_SCHED_PRESCALE_MASK , _IADC_SCHED_PRESCALE_SHIFT , _IADC_TIMER_TIMER_MASK , _IADC_TIMER_TIMER_SHIFT , IADC_Config_t::adcClkPrescale , IADC_Config_t::adcMode , IADC_Config_t::analogGain , IADC_CFG_TypeDef::CFG , IADC_TypeDef::CFG , IADC_TypeDef::CMPTHR , IADC_AllConfigs_t::configs , IADC_TypeDef::CTRL , IADC_Init_t::debugHalt , DEVINFO , IADC_Init_t::greaterThanEqualThres , IADC_calcAdcClkPrescale() , IADC_calcSrcClkPrescale() , IADC_calcTimebase() , IADC_CTRL_ADCCLKSUSPEND0 , IADC_CTRL_ADCCLKSUSPEND1 , IADC_CTRL_DBGHALT , IADC_SCALE_GAIN3MSB , iadcCfgModeNormal , IADC_Init_t::iadcClkSuspend0 , IADC_Init_t::iadcClkSuspend1 , IADC_Init_t::lessThanEqualThres , IADC_Config_t::osrHighSpeed , IADC_Config_t::reference , IADC_CFG_TypeDef::SCALE , IADC_CFG_TypeDef::SCHED , SL_MAX , IADC_Init_t::srcClkPrescale , IADC_Init_t::timebase , IADC_TypeDef::TIMER , IADC_Init_t::timerCycles , IADC_Config_t::twosComplement , IADC_Config_t::vRef , and IADC_Init_t::warmup .
| void IADC_initScan | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| const IADC_InitScan_t * | 
           
            init,
           
           | 
         ||
| const IADC_ScanTable_t * | 
           
            scanTable
           
           | 
         ||
| ) | 
Initialize IADC scan sequence.
This function will configure scan mode and set up entries in the scan table. The scan table mask can be updated by calling IADC_updateScanMask.
- Note
 - This function will stop any ongoing conversions.
 - If an even numbered pin is selected for the positive input, the negative input must use an odd numbered pin and vice versa.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] initPointer to IADC initialization structure. [in] scanTablePointer to IADC scan table structure.  
        Definition at line
        
         370
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_MASKREQ_MASKREQ_SHIFT , _IADC_SCAN_CFG_MASK , _IADC_SCAN_CFG_SHIFT , _IADC_SCAN_PINNEG_MASK , _IADC_SCAN_PINNEG_SHIFT , _IADC_SCAN_PINPOS_MASK , _IADC_SCAN_PINPOS_SHIFT , _IADC_SCAN_PORTNEG_MASK , _IADC_SCAN_PORTPOS_MASK , _IADC_SCANFIFOCFG_ALIGNMENT_MASK , _IADC_SCANFIFOCFG_ALIGNMENT_SHIFT , _IADC_SCANFIFOCFG_DVL_MASK , _IADC_SCANFIFOCFG_DVL_SHIFT , _IADC_TRIGGER_SCANTRIGACTION_MASK , _IADC_TRIGGER_SCANTRIGACTION_SHIFT , _IADC_TRIGGER_SCANTRIGSEL_MASK , _IADC_TRIGGER_SCANTRIGSEL_SHIFT , IADC_InitScan_t::alignment , IADC_ScanTableEntry_t::compare , IADC_ScanTableEntry_t::configId , IADC_InitScan_t::dataValidLevel , IADC_ScanTable_t::entries , IADC_InitScan_t::fifoDmaWakeup , IADC_command() , IADC_SCAN_CMP , IADC_SCANFIFOCFG_DMAWUFIFOSCAN , IADC_SCANFIFOCFG_SHOWID , iadcCmdStartScan , IADC_ScanTableEntry_t::includeInScan , IADC_TypeDef::MASKREQ , IADC_ScanTableEntry_t::negInput , IADC_ScanTableEntry_t::posInput , IADC_SCANTABLE_TypeDef::SCAN , IADC_TypeDef::SCANFIFOCFG , IADC_TypeDef::SCANTABLE , IADC_InitScan_t::showId , IADC_InitScan_t::start , IADC_TypeDef::TRIGGER , IADC_InitScan_t::triggerAction , and IADC_InitScan_t::triggerSelect .
| void IADC_initSingle | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| const IADC_InitSingle_t * | 
           
            init,
           
           | 
         ||
| const IADC_SingleInput_t * | 
           
            input
           
           | 
         ||
| ) | 
Initialize single IADC conversion.
This function will initialize the single conversion and configure the single input selection.
- Note
 - This function will stop any ongoing conversions.
 - If an even numbered pin is selected for the positive input, the negative input must use an odd numbered pin and vice versa.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] initPointer to IADC single initialization structure. [in] singleInputPointer to IADC single input selection initialization structure.  
        Definition at line
        
         445
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_SINGLEFIFOCFG_ALIGNMENT_MASK , _IADC_SINGLEFIFOCFG_ALIGNMENT_SHIFT , _IADC_SINGLEFIFOCFG_DVL_MASK , _IADC_SINGLEFIFOCFG_DVL_SHIFT , _IADC_TRIGGER_SINGLETAILGATE_MASK , _IADC_TRIGGER_SINGLETRIGACTION_MASK , _IADC_TRIGGER_SINGLETRIGACTION_SHIFT , _IADC_TRIGGER_SINGLETRIGSEL_MASK , _IADC_TRIGGER_SINGLETRIGSEL_SHIFT , IADC_InitSingle_t::alignment , IADC_InitSingle_t::dataValidLevel , IADC_InitSingle_t::fifoDmaWakeup , IADC_command() , IADC_SINGLEFIFOCFG_DMAWUFIFOSINGLE , IADC_SINGLEFIFOCFG_SHOWID , IADC_TRIGGER_SINGLETAILGATE , IADC_updateSingleInput() , iadcCmdStartSingle , IADC_InitSingle_t::showId , IADC_TypeDef::SINGLEFIFOCFG , IADC_InitSingle_t::singleTailgate , IADC_InitSingle_t::start , IADC_TypeDef::TRIGGER , IADC_InitSingle_t::triggerAction , and IADC_InitSingle_t::triggerSelect .
| __STATIC_INLINE IADC_NegInput_t IADC_portPinToNegInput | ( | GPIO_Port_TypeDef | 
           
            port,
           
           | 
         
| uint8_t | 
           
            pin
           
           | 
         ||
| ) | 
Convert GPIO port/pin to IADC negative input selection.
- Parameters
 - 
         
[in] portGPIO port [in] pinGPIO in  
- Returns
 - IADC negative input selection
 
        Definition at line
        
         1142
        
        of file
        
         em_iadc.h
        
        .
       
References _IADC_SCAN_PORTNEG_PORTA .
| __STATIC_INLINE IADC_PosInput_t IADC_portPinToPosInput | ( | GPIO_Port_TypeDef | 
           
            port,
           
           | 
         
| uint8_t | 
           
            pin
           
           | 
         ||
| ) | 
Convert GPIO port/pin to IADC positive input selection.
- Parameters
 - 
         
[in] portGPIO port [in] pinGPIO in  
- Returns
 - IADC positive input selection
 
        Definition at line
        
         1163
        
        of file
        
         em_iadc.h
        
        .
       
References _IADC_SCAN_PORTPOS_PORTA .
| __STATIC_INLINE uint32_t IADC_pullScanFifoData | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Pull data from scan data FIFO. If showId was set for the scan entry initialization, the data will contain the ID of the scan entry.
- Note
 - Check data valid flag before calling this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Scan conversion data.
 
        Definition at line
        
         904
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::SCANFIFODATA .
Referenced by IADC_reset() .
| IADC_Result_t IADC_pullScanFifoResult | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Pull result from scan data FIFO. The result struct includes both the data and the ID (0x20) if showId was set when initializing scan entry.
- Note
 - Check data valid flag before calling this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Scan conversion result struct holding data and id.
 
        Definition at line
        
         904
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_SCANFIFOCFG_ALIGNMENT_MASK , _IADC_SCANFIFOCFG_ALIGNMENT_SHIFT , IADC_TypeDef::SCANFIFOCFG , and IADC_TypeDef::SCANFIFODATA .
| __STATIC_INLINE uint32_t IADC_pullSingleFifoData | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Pull data from single data FIFO. If showId was set when initializing single mode, the results will contain the ID (0x20).
- Note
 - Check data valid flag before calling this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Single conversion data.
 
        Definition at line
        
         865
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::SINGLEFIFODATA .
Referenced by IADC_reset() .
| IADC_Result_t IADC_pullSingleFifoResult | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Pull result from single data FIFO. The result struct includes both the data and the ID (0x20) if showId was set when initializing single mode.
- Note
 - Check data valid flag before calling this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Single conversion result struct holding data and id.
 
        Definition at line
        
         859
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_SINGLEFIFOCFG_ALIGNMENT_MASK , _IADC_SINGLEFIFOCFG_ALIGNMENT_SHIFT , IADC_TypeDef::SINGLEFIFOCFG , and IADC_TypeDef::SINGLEFIFODATA .
| __STATIC_INLINE uint32_t IADC_readScanData | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Read most recent scan conversion data. If showId was set for the scan entry initialization, the data will contain the ID of the scan entry. Calling this function will not affect the state of the scan data FIFO.
- Note
 - Check data valid flag before calling this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Scan conversion data.
 
        Definition at line
        
         924
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::SCANDATA .
Referenced by IADC_reset() .
| IADC_Result_t IADC_readScanResult | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Read most recent scan conversion result. The result struct includes both the data and the ID (0x20) if showId was set when initializing scan entry. Calling this function will not affect the state of the scan data FIFO.
- Note
 - Check data valid flag before calling this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Scan conversion result struct holding data and id.
 
        Definition at line
        
         927
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_SCANFIFOCFG_ALIGNMENT_MASK , _IADC_SCANFIFOCFG_ALIGNMENT_SHIFT , IADC_TypeDef::SCANDATA , and IADC_TypeDef::SCANFIFOCFG .
| __STATIC_INLINE uint32_t IADC_readSingleData | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Read most recent single conversion data. If showId was set when initializing single mode, the data will contain the ID (0x20). Calling this function will not affect the state of the single data FIFO.
- Note
 - Check data valid flag before calling this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Single conversion data.
 
        Definition at line
        
         885
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::SINGLEDATA .
Referenced by IADC_reset() .
| IADC_Result_t IADC_readSingleResult | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Read most recent single conversion result. The result struct includes both the data and the ID (0x20) if showId was set when initializing single mode. Calling this function will not affect the state of the single data FIFO.
- Note
 - Check data valid flag before calling this function.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
- Returns
 - Single conversion result struct holding data and id.
 
        Definition at line
        
         882
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_SINGLEFIFOCFG_ALIGNMENT_MASK , _IADC_SINGLEFIFOCFG_ALIGNMENT_SHIFT , IADC_TypeDef::SINGLEDATA , and IADC_TypeDef::SINGLEFIFOCFG .
| void IADC_reset | ( | IADC_TypeDef * | 
           
            iadc
           
           | 
          ) | 
Reset IADC to same state as after a HW reset.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block.  
        Definition at line
        
         624
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_CFG_RESETVALUE , _IADC_CMPTHR_RESETVALUE , _IADC_CTRL_RESETVALUE , _IADC_IEN_MASK , _IADC_IF_MASK , _IADC_MASKREQ_RESETVALUE , _IADC_SCALE_RESETVALUE , _IADC_SCAN_RESETVALUE , _IADC_SCANFIFOCFG_RESETVALUE , _IADC_SCHED_RESETVALUE , _IADC_SINGLE_RESETVALUE , _IADC_SINGLEFIFOCFG_RESETVALUE , _IADC_TIMER_RESETVALUE , _IADC_TRIGGER_RESETVALUE , IADC_CFG_TypeDef::CFG , IADC_TypeDef::CFG , IADC_TypeDef::CMD , IADC_TypeDef::CMPTHR , IADC_TypeDef::CTRL , IADC_clearInt() , IADC_CMD_SCANSTOP , IADC_CMD_SINGLESTOP , IADC_CMD_TIMERDIS , IADC_disableInt() , IADC_pullScanFifoData() , IADC_pullSingleFifoData() , IADC_readScanData() , IADC_readSingleData() , IADC_STATUS_CONVERTING , IADC_STATUS_MASKREQWRITEPENDING , IADC_STATUS_SCANFIFODV , IADC_STATUS_SCANQUEUEPENDING , IADC_STATUS_SINGLEFIFODV , IADC_STATUS_SINGLEQUEUEPENDING , IADC_STATUS_SINGLEWRITEPENDING , IADC_STATUS_TIMERACTIVE , IADC_TypeDef::MASKREQ , IADC_CFG_TypeDef::SCALE , IADC_SCANTABLE_TypeDef::SCAN , IADC_TypeDef::SCANFIFOCFG , IADC_TypeDef::SCANTABLE , IADC_CFG_TypeDef::SCHED , IADC_TypeDef::SINGLE , IADC_TypeDef::SINGLEFIFOCFG , IADC_TypeDef::STATUS , IADC_TypeDef::TIMER , and IADC_TypeDef::TRIGGER .
| __STATIC_INLINE void IADC_setInt | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint32_t | 
           
            flags
           
           | 
         ||
| ) | 
Set one or more pending IADC interrupts from SW.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] flagsIADC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the IADC module (IADC_IF_nnn).  
        Definition at line
        
         1047
        
        of file
        
         em_iadc.h
        
        .
       
References IADC_TypeDef::IF_SET .
| void IADC_setScanMask | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint32_t | 
           
            mask
           
           | 
         ||
| ) | 
Set mask of IADC scan table entries to include in scan.
Set mask of scan table entries to include in next scan. This function can be called while scan conversions are ongoing, but the new scan mask will take effect once the ongoing scan is completed.
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] maskMask of scan table entries to include in scan.  
        Definition at line
        
         538
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_MASKREQ_MASKREQ_MASK , _IADC_MASKREQ_MASKREQ_SHIFT , IADC_TypeDef::EN , IADC_EN_EN , and IADC_TypeDef::MASKREQ .
| void IADC_updateScanEntry | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| uint8_t | 
           
            id,
           
           | 
         ||
| IADC_ScanTableEntry_t * | 
           
            entry
           
           | 
         ||
| ) | 
Add/update entry in scan table.
This function will update or add an entry in the scan table with a specific ID.
- Note
 - This function will stop any ongoing conversions.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] idId of scan table entry to add. [in] entryPointer to scan table entry structure.  
        Definition at line
        
         580
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_MASKREQ_MASKREQ_SHIFT , _IADC_SCAN_CFG_MASK , _IADC_SCAN_CFG_SHIFT , _IADC_SCAN_PINNEG_MASK , _IADC_SCAN_PINNEG_SHIFT , _IADC_SCAN_PINPOS_MASK , _IADC_SCAN_PINPOS_SHIFT , _IADC_SCAN_PORTNEG_MASK , _IADC_SCAN_PORTPOS_MASK , IADC_ScanTableEntry_t::compare , IADC_ScanTableEntry_t::configId , IADC_TypeDef::EN , IADC_EN_EN , IADC_SCAN_CMP , IADC_ScanTableEntry_t::includeInScan , IADC_TypeDef::MASKREQ_CLR , IADC_TypeDef::MASKREQ_SET , IADC_ScanTableEntry_t::negInput , IADC_ScanTableEntry_t::posInput , IADC_SCANTABLE_TypeDef::SCAN , and IADC_TypeDef::SCANTABLE .
| void IADC_updateSingleInput | ( | IADC_TypeDef * | 
           
            iadc,
           
           | 
         
| const IADC_SingleInput_t * | 
           
            input
           
           | 
         ||
| ) | 
Update IADC single input selection.
This function updates the single input selection. The function can be called while single and/or scan conversions are ongoing and the new input configuration will take place on the next single conversion.
- Note
 - If an even numbered pin is selected for the positive input, the negative input must use an odd numbered pin and vice versa.
 
- Parameters
 - 
         
[in] iadcPointer to IADC peripheral register block. [in] inputPointer to single input selection structure.  
        Definition at line
        
         497
        
        of file
        
         em_iadc.c
        
        .
       
References _IADC_SINGLE_CFG_MASK , _IADC_SINGLE_CFG_SHIFT , _IADC_SINGLE_PINNEG_MASK , _IADC_SINGLE_PINNEG_SHIFT , _IADC_SINGLE_PINPOS_MASK , _IADC_SINGLE_PINPOS_SHIFT , _IADC_SINGLE_PORTNEG_MASK , _IADC_SINGLE_PORTPOS_MASK , IADC_SingleInput_t::compare , IADC_SingleInput_t::configId , IADC_TypeDef::EN , IADC_EN_EN , IADC_SINGLE_CMP , IADC_SingleInput_t::negInput , IADC_SingleInput_t::posInput , and IADC_TypeDef::SINGLE .
Referenced by IADC_initSingle() .