SE_Status_t Struct ReferenceEMLIB > SE
       Definition at line
       
        342
       
       of file
       
        em_se.h
       
       .
      
         Data Fields | 
       |
| uint32_t | bootStatus | 
| SE_DebugStatus_t | debugStatus | 
| uint32_t | hostFwVersion | 
| bool | secureBootEnabled | 
| uint32_t | seFwVersion | 
Field Documentation
| uint32_t SE_Status_t::bootStatus | 
Boot status code / error code (Bits [7:0]).
        Definition at line
        
         344
        
        of file
        
         em_se.h
        
        .
       
Referenced by SE_getStatus() .
| SE_DebugStatus_t SE_Status_t::debugStatus | 
| uint32_t SE_Status_t::hostFwVersion | 
Host firmware version (if available).
        Definition at line
        
         348
        
        of file
        
         em_se.h
        
        .
       
Referenced by SE_getStatus() .
| bool SE_Status_t::secureBootEnabled | 
| uint32_t SE_Status_t::seFwVersion | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/emlib/inc/
       
em_se.h