GPIO_PRSROUTE_TypeDef Struct ReferenceDevices
Definition at line
91
of file
efr32mg21_gpio.h
.
Data Fields |
|
| __IOM uint32_t | ASYNCH0ROUTE |
| __IOM uint32_t | ASYNCH10ROUTE |
| __IOM uint32_t | ASYNCH11ROUTE |
| __IOM uint32_t | ASYNCH1ROUTE |
| __IOM uint32_t | ASYNCH2ROUTE |
| __IOM uint32_t | ASYNCH3ROUTE |
| __IOM uint32_t | ASYNCH4ROUTE |
| __IOM uint32_t | ASYNCH5ROUTE |
| __IOM uint32_t | ASYNCH6ROUTE |
| __IOM uint32_t | ASYNCH7ROUTE |
| __IOM uint32_t | ASYNCH8ROUTE |
| __IOM uint32_t | ASYNCH9ROUTE |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | ROUTEEN |
| __IOM uint32_t | SYNCH0ROUTE |
| __IOM uint32_t | SYNCH1ROUTE |
| __IOM uint32_t | SYNCH2ROUTE |
| __IOM uint32_t | SYNCH3ROUTE |
Field Documentation
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH0ROUTE |
ASYNCH0 port/pin select
Definition at line
93
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH10ROUTE |
ASYNCH10 port/pin select
Definition at line
103
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH11ROUTE |
ASYNCH11 port/pin select
Definition at line
104
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH1ROUTE |
ASYNCH1 port/pin select
Definition at line
94
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH2ROUTE |
ASYNCH2 port/pin select
Definition at line
95
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH3ROUTE |
ASYNCH3 port/pin select
Definition at line
96
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH4ROUTE |
ASYNCH4 port/pin select
Definition at line
97
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH5ROUTE |
ASYNCH5 port/pin select
Definition at line
98
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH6ROUTE |
ASYNCH6 port/pin select
Definition at line
99
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH7ROUTE |
ASYNCH7 port/pin select
Definition at line
100
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH8ROUTE |
ASYNCH8 port/pin select
Definition at line
101
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH9ROUTE |
ASYNCH9 port/pin select
Definition at line
102
of file
efr32mg21_gpio.h
.
| uint32_t GPIO_PRSROUTE_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
109
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::ROUTEEN |
PRS0 pin enable
Definition at line
92
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::SYNCH0ROUTE |
SYNCH0 port/pin select
Definition at line
105
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::SYNCH1ROUTE |
SYNCH1 port/pin select
Definition at line
106
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::SYNCH2ROUTE |
SYNCH2 port/pin select
Definition at line
107
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_PRSROUTE_TypeDef::SYNCH3ROUTE |
SYNCH3 port/pin select
Definition at line
108
of file
efr32mg21_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_gpio.h