GPIO_ACMPROUTE_TypeDef Struct ReferenceDevices
Definition at line
44
of file
efr32mg21_gpio.h
.
Data Fields |
|
| __IOM uint32_t | ACMPOUTROUTE |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | ROUTEEN |
Field Documentation
| __IOM uint32_t GPIO_ACMPROUTE_TypeDef::ACMPOUTROUTE |
ACMPOUT port/pin select
Definition at line
46
of file
efr32mg21_gpio.h
.
| uint32_t GPIO_ACMPROUTE_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
47
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_ACMPROUTE_TypeDef::ROUTEEN |
ACMP0 pin enable
Definition at line
45
of file
efr32mg21_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_gpio.h