AES_TypeDef Struct ReferenceDevices > AES
AES Register Declaration.
Definition at line
47
of file
efr32mg21_aes.h
.
#include <
efr32mg21_aes.h
>
Data Fields |
|
| __IOM uint32_t | CMD |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | FETCHADDR |
| __IOM uint32_t | FETCHDESCR |
| __IOM uint32_t | FETCHLEN |
| __IOM uint32_t | FETCHTAG |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | PUSHADDR |
| __IOM uint32_t | PUSHDESCR |
| __IOM uint32_t | PUSHLEN |
| uint32_t | RESERVED0 [2U] |
| uint32_t | RESERVED1 [1U] |
| uint32_t | RESERVED2 [4079U] |
| uint32_t | RESERVED3 [1U] |
| __IM uint32_t | STATUS |
Field Documentation
| __IOM uint32_t AES_TypeDef::CMD |
Command register
Definition at line
61
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::CTRL |
Control register
Definition at line
60
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::FETCHADDR |
Fetcher Address
Definition at line
48
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::FETCHDESCR |
Fetcher Descriptor
Definition at line
49
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::FETCHLEN |
Fetcher Length
Definition at line
50
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::FETCHTAG |
Fetcher Tag
Definition at line
51
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::IEN |
Interrupt Enable
Definition at line
55
of file
efr32mg21_aes.h
.
| __IM uint32_t AES_TypeDef::IF |
Interrupt Flags
Definition at line
57
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::IFC |
Interrupt status clear
Definition at line
59
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::PUSHADDR |
Pusher Address
Definition at line
52
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::PUSHDESCR |
Pusher Descriptor
Definition at line
53
of file
efr32mg21_aes.h
.
| __IOM uint32_t AES_TypeDef::PUSHLEN |
Pusher Length
Definition at line
54
of file
efr32mg21_aes.h
.
| uint32_t AES_TypeDef::RESERVED0[2U] |
Reserved for future use
Definition at line
56
of file
efr32mg21_aes.h
.
| uint32_t AES_TypeDef::RESERVED1[1U] |
Reserved for future use
Definition at line
58
of file
efr32mg21_aes.h
.
| uint32_t AES_TypeDef::RESERVED2[4079U] |
Reserved for future use
Definition at line
63
of file
efr32mg21_aes.h
.
| uint32_t AES_TypeDef::RESERVED3[1U] |
Reserved for future use
Definition at line
64
of file
efr32mg21_aes.h
.
| __IM uint32_t AES_TypeDef::STATUS |
Status register
Definition at line
62
of file
efr32mg21_aes.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_aes.h