IADC_SingleInput_t Struct ReferenceEMLIB > IADC
IADC single input selection structure
Definition at line
748
of file
em_iadc.h
.
#include <
em_iadc.h
>
Data Fields |
|
| bool | compare |
| uint8_t | configId |
| IADC_NegInput_t | negInput |
| IADC_PosInput_t | posInput |
Field Documentation
| bool IADC_SingleInput_t::compare |
Perform digital window comparison on the result from this entry.
Definition at line
752
of file
em_iadc.h
.
Referenced by IADC_updateSingleInput() .
| uint8_t IADC_SingleInput_t::configId |
Configuration id.
Definition at line
751
of file
em_iadc.h
.
Referenced by IADC_updateSingleInput() .
| IADC_NegInput_t IADC_SingleInput_t::negInput |
Port/pin input for the negative side of the ADC.
Definition at line
749
of file
em_iadc.h
.
Referenced by IADC_updateSingleInput() .
| IADC_PosInput_t IADC_SingleInput_t::posInput |
Port/pin input for the positive side of the ADC.
Definition at line
750
of file
em_iadc.h
.
Referenced by IADC_updateSingleInput() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_iadc.h