BUFC_BUF_TypeDef Struct ReferenceDevices > BUFC
BUFC BUF Register Group Declaration.
Definition at line
48
of file
efr32mg21_bufc.h
.
#include <
efr32mg21_bufc.h
>
Data Fields |
|
| __IOM uint32_t | ADDR |
| __IOM uint32_t | CMD |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | FIFOASYNC |
| __IM uint32_t | READDATA |
| __IOM uint32_t | READOFFSET |
| uint32_t | RESERVED0 [1U] |
| __IM uint32_t | STATUS |
| __IOM uint32_t | THRESHOLDCTRL |
| __IOM uint32_t | WRITEDATA |
| __IOM uint32_t | WRITEOFFSET |
| __IOM uint32_t | XWRITE |
Field Documentation
| __IOM uint32_t BUFC_BUF_TypeDef::ADDR |
Buffer Address
Definition at line
50
of file
efr32mg21_bufc.h
.
| __IOM uint32_t BUFC_BUF_TypeDef::CMD |
Buffer Command
Definition at line
59
of file
efr32mg21_bufc.h
.
| __IOM uint32_t BUFC_BUF_TypeDef::CTRL |
Buffer Control
Definition at line
49
of file
efr32mg21_bufc.h
.
| __IOM uint32_t BUFC_BUF_TypeDef::FIFOASYNC |
New Register
Definition at line
60
of file
efr32mg21_bufc.h
.
| __IM uint32_t BUFC_BUF_TypeDef::READDATA |
Buffer Read Data
Definition at line
54
of file
efr32mg21_bufc.h
.
| __IOM uint32_t BUFC_BUF_TypeDef::READOFFSET |
Read Offset
Definition at line
52
of file
efr32mg21_bufc.h
.
| uint32_t BUFC_BUF_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
53
of file
efr32mg21_bufc.h
.
| __IM uint32_t BUFC_BUF_TypeDef::STATUS |
Buffer Status Register
Definition at line
57
of file
efr32mg21_bufc.h
.
| __IOM uint32_t BUFC_BUF_TypeDef::THRESHOLDCTRL |
Threshold Control
Definition at line
58
of file
efr32mg21_bufc.h
.
| __IOM uint32_t BUFC_BUF_TypeDef::WRITEDATA |
Buffer Write Data
Definition at line
55
of file
efr32mg21_bufc.h
.
| __IOM uint32_t BUFC_BUF_TypeDef::WRITEOFFSET |
Write Offset
Definition at line
51
of file
efr32mg21_bufc.h
.
| __IOM uint32_t BUFC_BUF_TypeDef::XWRITE |
Buffer XOR Write
Definition at line
56
of file
efr32mg21_bufc.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_bufc.h