FSRCO_TypeDef Struct ReferenceDevices > FSRCO
FSRCO Register Declaration.
Definition at line
48
of file
efr32mg21_fsrco.h
.
#include <
efr32mg21_fsrco.h
>
Data Fields |
|
| __IM uint32_t | IPVERSION |
| __IM uint32_t | IPVERSION_CLR |
| __IM uint32_t | IPVERSION_SET |
| __IM uint32_t | IPVERSION_TGL |
| uint32_t | RESERVED0 [1023U] |
| uint32_t | RESERVED1 [1023U] |
| uint32_t | RESERVED2 [1023U] |
Field Documentation
| __IM uint32_t FSRCO_TypeDef::IPVERSION |
IP Version
Definition at line
49
of file
efr32mg21_fsrco.h
.
| __IM uint32_t FSRCO_TypeDef::IPVERSION_CLR |
IP Version
Definition at line
53
of file
efr32mg21_fsrco.h
.
| __IM uint32_t FSRCO_TypeDef::IPVERSION_SET |
IP Version
Definition at line
51
of file
efr32mg21_fsrco.h
.
| __IM uint32_t FSRCO_TypeDef::IPVERSION_TGL |
IP Version
Definition at line
55
of file
efr32mg21_fsrco.h
.
| uint32_t FSRCO_TypeDef::RESERVED0[1023U] |
Reserved for future use
Definition at line
50
of file
efr32mg21_fsrco.h
.
| uint32_t FSRCO_TypeDef::RESERVED1[1023U] |
Reserved for future use
Definition at line
52
of file
efr32mg21_fsrco.h
.
| uint32_t FSRCO_TypeDef::RESERVED2[1023U] |
Reserved for future use
Definition at line
54
of file
efr32mg21_fsrco.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_fsrco.h