GPIO_MODEMROUTE_TypeDef Struct ReferenceDevices
Definition at line
81
of file
efr32mg21_gpio.h
.
Data Fields |
|
| __IOM uint32_t | ANT0ROUTE |
| __IOM uint32_t | ANT1ROUTE |
| __IOM uint32_t | DCLKROUTE |
| __IOM uint32_t | DINROUTE |
| __IOM uint32_t | DOUTROUTE |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | ROUTEEN |
Field Documentation
| __IOM uint32_t GPIO_MODEMROUTE_TypeDef::ANT0ROUTE |
ANT0 port/pin select
Definition at line
83
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_MODEMROUTE_TypeDef::ANT1ROUTE |
ANT1 port/pin select
Definition at line
84
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_MODEMROUTE_TypeDef::DCLKROUTE |
DCLK port/pin select
Definition at line
85
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_MODEMROUTE_TypeDef::DINROUTE |
DIN port/pin select
Definition at line
86
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_MODEMROUTE_TypeDef::DOUTROUTE |
DOUT port/pin select
Definition at line
87
of file
efr32mg21_gpio.h
.
| uint32_t GPIO_MODEMROUTE_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
88
of file
efr32mg21_gpio.h
.
| __IOM uint32_t GPIO_MODEMROUTE_TypeDef::ROUTEEN |
MODEM pin enable
Definition at line
82
of file
efr32mg21_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32MG21/Include/
efr32mg21_gpio.h