BCP_Packet_ Struct ReferenceBSP > API for STKs and WSTKs

BCP Packet Structure - Board controller communication protocol version 1.

Definition at line 75 of file bsp_bcp.h .

#include < bsp_bcp.h >

Data Fields

uint8_t data [ BSP_BCP_PACKET_SIZE ]
uint8_t magic
uint8_t payloadLength
uint8_t type

Field Documentation

uint8_t BCP_Packet_::data[ BSP_BCP_PACKET_SIZE ]

BCP Packet Data payload

Definition at line 79 of file bsp_bcp.h .

uint8_t BCP_Packet_::magic

Magic - start of packet - must be BSP_BCP_MAGIC

Definition at line 76 of file bsp_bcp.h .

uint8_t BCP_Packet_::payloadLength

Length of data segment >=0 and <=BSP_BCP_PACKET_SIZE

Definition at line 78 of file bsp_bcp.h .

uint8_t BCP_Packet_::type

Type of packet

Definition at line 77 of file bsp_bcp.h .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/hardware/kit/common/bsp/ bsp_bcp.h