Receive_PluginEMDRV > EZRADIODRV > Plugin_System
Detailed Description
Receive plugin, see Plugin System Layer for detailed documentation.
.
         Data Structures | 
       |
| struct | EZRADIODRV_PacketRxHandle | 
| 
         EzRadio receive plug-in instance initialization and handler structure.
          | 
       |
         Macros | 
       |
| #define | EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT | 
| 
         Configuration data for EzRadio receive plug-in.
          | 
       |
         Typedefs | 
       |
| typedef struct EZRADIODRV_PacketRxHandle | EZRADIODRV_PacketRxHandle_t | 
| 
         EzRadio receive plug-in instance initialization and handler structure.
          | 
       |
         Functions | 
       |
| Ecode_t | ezradioStartRx ( EZRADIODRV_Handle_t radioHandle) | 
| 
         Set Radio to RX mode, packet length is always coming from the radio configuration.
          | 
       |
Macro Definition Documentation
| #define EZRADIODRV_RECEIVE_PLUGIN_INIT_DEFAULT | 
Configuration data for EzRadio receive plug-in.
        Definition at line
        
         59
        
        of file
        
         ezradio_receive_plugin.h
        
        .
       
Function Documentation
| Ecode_t ezradioStartRx | ( | EZRADIODRV_Handle_t | 
           
            radioHandle
           
           | 
          ) | 
Set Radio to RX mode, packet length is always coming from the radio configuration.
- Parameters
 - 
         
radioHandleHandler of the EzRadio driver instance where packet buffer, callback and channel configurations are set.  
- Returns
 - ECODE_EMDRV_EZRADIODRV_OK on success. On failure an appropriate EZRADIODRV Ecode_t is returned.
 
        Definition at line
        
         49
        
        of file
        
         ezradio_receive_plugin.c
        
        .
       
References EZRADIODRV_PacketRxHandle::channel , ECODE_EMDRV_EZRADIODRV_OK , ezradio_start_rx() , and EZRADIODRV_HandleData::packetRx .